hi all
i m trying to use huawei e303 3G modem on beaglebaord and android gingerbread
the problem is when ever i connect the modem it is not creating any interfaces in /dev directory
i have enabled below things in the kernel configuration : linux-2.6.37
*] Network device support --->
<*> PPP (point-to-point protocol) support
<*> PPP BSD-Compress compression
<*> PPP Deflate compression
<*> PPP support for async serial ports
<*> PPP support for sync tty ports [*]
USB support --->
<*> USB Modem (CDC ACM) support <*>
USB Serial Converter support --->
[*] USB Generic Serial Driver
<*> USB driver for GSM and CDMA modems ( i couldnt find this on linux 2.6.37)
on ubuntu 10.04 it is creating all required interfaces and working fine ...
kindly help..