This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

System Analyzer - C6678 - Image Processing Demo

Guru 10750 points


Hi,

I'm trying to run the System Analyzer on the C6678 Image Processing Demo with not too much success, I have started the System Analyzer live before the process and than when I want to see for example the execution graph I get "Showing 0 records | Processing 0%" I have noticed that the file systemAnalyzerData.bin size is "0" anything else I need to do to start the data collection?

I'm using CCS 5.2.1.00018, MCUSDK 2.1.1.4, UIA 1.1.0.4, BIOS 6.33.6.50

Thanks,

HR