This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems about HUA demo



Hi everyone,

    I have verified that HUA demo runs well on C6678 EVM. However,when i loaded  hua_evmc6678l.out to the C6678 DSP

on my own board, It ran  automatically without my pressing the run button. And nothing was printed in the console window.

I suspended the routine,then found it stayed in EVM_init() / platform_init() / Init_SGMII() / CSL_SGMII_getStatus() and could not step out.

I didn't modify anything of the HUA app. Why did this happen ?

    In hpdspua.c,it says that " If you are debuggging within CCS the default option in your target configuration file may be to executer all

code up untill Main as the image loads. To debug this , you should disable that option." But i can't find where to set the option mentioned above.

Is this the cause for HUA app running automatically as soon as it is loaded?

     In addtion,there are two differences between our board and C6678 EVM, whicn ,I think,may  not  be  the cause of the problem .

    1)The input clock freq for GbE is 156.25MHz

    2)We connect the PHY device to SGMII 0 of C6678, but PHY is connected to SGMII 1 on C6678 EVM.

    Hope someone heips. Thank you in advance.

Best Regards

Nuoxi

Library  veision :

mcsdk_2_00_09_21

pdk_C6678_1_0_0_21