Hi all,
I am working with PSP 3.22.0.02 on OMAPL138. Having trouble getting rootfs mount over NFS.
I have the NFS server set up on my Ubuntu development machine and I could the EVM to mount rootfs over NFS when using the DVSDK (ti-dvsdk_omapl138-evm_04_03_00_06)
But, I am moving to PSP 3.22.0.02, but having trouble mounting rootfs
I am referring to
http://processors.wiki.ti.com/index.php/GSG:_Setting_up_OMAP-L1/AM1x_Target_File_System
to get the rootfs. I am looking at the link in the section which talks about how to set up targetfs for PSP versions greater than 3.20.00.11
The board boots up (using tftpboot), but cannot find the NFS server. Wondering if there are any NFS version differences with the latest PSP which is causing trouble or if that rootfs from the above page is not the correct one for PSP version 3.22.0.02
Can you please let me know when you get a chance?