Other Parts Discussed in Thread: DM3730
Hi,
I am in use of DM3730 platform, recently ,I encounted a problem with the Network. The problem is as follows:
1. when I connect the platform with net wire before the board powered on, the network works well.
2. When I disconnect the platform with the net wire before the board powered on , and I change the IP address and rebind the network adapter to recognize the new IP by using API function, then network will not work anymore unless the board powered on again .
so ,the problem can concluded as this , the network doesn't work if the network adapter was rebinded when the system powered on with the net wire disconnected .
do you know what happened?
Hope for your reply
Liuyan from NovaStar company.