This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mt9p031 can't rebooted



Hi all,

I have encounter a problem of reboot. My customer board of ipnc is based on dm365 EVM,
which is using mt9p031. All are OK if I boot the system from power on.

But if I boot it from linux command "reboot", the capture process is frozen at beginning.
I guess the mt9p031 not reset to the proper status. I have written RESET register of mt9p031
at start of the program, it seems no effect.

Does anybody encounter the same problem ? any solution ? any cue ?

The system is DM368 + MT9P031 + DVSDK 4.0.2

Any help appreciated !

Yang