This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 CSL emif support



I've been using the CSL to develop for the C5515, but have struggled to find emif support. 

There is a cslr_emif.h file, which contains the register definitions, but no csl_emif.c or csl_emif.h. These files are referenced and used in sample code online, but I can't seem to find them in the latest version of the csl (verson 3.00) or the previous version. Has the emif support been removed from the CSL libraries, and if so, is there another way for me to easily configure the SDRAM without having to reinvent the wheel? 

  • CSL's emif support has been currently removed from the package. There are plans to reincorporate support in future releases. 

    For now, we do have a couple of files for debugging purposes (not a polished example, only the basics) that you can use if you'd like. 

    7345.dbg_sdram.h

    /*
     * $$$MODULE_NAME dbg_sdram.c
     *
     * $$$MODULE_DESC dbg_sdram.c
     *
     * Copyright (C) 2011 Texas Instruments Incorporated - http://www.ti.com/
     *
     *  This software is licensed under the  standard terms and conditions in the Texas Instruments  Incorporated
     *  Technology and Software Publicly Available Software License Agreement , a copy of which is included in the
     *  software download.
    */
    
    #include <std.h>
    #include "soc.h"
    #include "dbg_sdram.h"
    
    Int16 *sdramBasePtr0;
    Int16 *sdramPtr0;
    Int16 *sdramBasePtr1;
    Int16 *sdramPtr1;
    
    Uint32 sdram_cntr;
    Uint32 sdram_flag;
    
    /* Congures EMIF/SDRAM */
    void initSdram(
        Bool fillMem, 
        Int16 fillMemVal
    )
    {
        Uint32 i;
        Uint16 reg;
        volatile ioport Uint16 *pReg;
        Int16 *sdram_ptr;
    
        /* Congure EMIF/SDRAM */
        CSL_FINST(CSL_SYSCTRL_REGS->SDRAMCCR, SYS_SDRAMCCR_SDCLK_EN, SDCLKOFF);
        for(i=0;i<20000;i++);
        CSL_FINST(CSL_SYSCTRL_REGS->ESCR, SYS_ESCR_BYTEMODE, FULL);
        reg = CSL_FMK(EMIF_SDTIMR1_TRAS, 0x3) |
            CSL_FMK(EMIF_SDTIMR1_TRC, 0x5) |
            CSL_FMK(EMIF_SDTIMR1_TRRD, 0x1);
        CSL_EMIF_REGS->SDTIMR1 = reg;
        pReg = (volatile ioport Uint16 *)EMIF_SDTIMR2;
        *pReg = (EMIF_SDTIMR2_TRFC_VAL << 11) |
            (EMIF_SDTIMR2_TRP_VAL << 8) |
            (EMIF_SDTIMR2_TRCD_VAL << 4) |
            (EMIF_SDTIMR2_TWR_VAL << 0); /* 0x4225 */
        reg = CSL_FMK(EMIF_SDCR1_NM, 0x1) |
            CSL_FMKT(EMIF_SDCR1_CL, THREE) |
            CSL_FMKT(EMIF_SDCR1_BIT_11_9_LOCK, WRITES) |
            CSL_FMKT(EMIF_SDCR1_IBANK, FOUR) |
            CSL_FMKT(EMIF_SDCR1_EBANK, ONE) |
            CSL_FMKT(EMIF_SDCR1_PAGESIZE, EIGHT);
        CSL_EMIF_REGS->SDCR1 = reg;
        reg = CSL_FMKT(EMIF_SDCR2_SR, EXIT) |
            CSL_FMKT(EMIF_SDCR2_PD, EXIT) |
            CSL_FMKT(EMIF_SDCR2_PDWR, NOREFR) |
            CSL_FMKT(EMIF_SDCR2_PASR, FOUR) |
            CSL_FMKT(EMIF_SDCR2_ROWSIZE, TWELVE) |
            CSL_FMK(EMIF_SDCR2_IBANK_POS, 0x0) |
            CSL_FMKT(EMIF_SDCR2_SDRAM_DRIVE, FULL) |
            CSL_FMKT(EMIF_SDCR2_BIT_9_1_LOCK, WRITES);
        CSL_EMIF_REGS->SDCR2 = reg;
        for (i=0; i<2048; i++);
    
        /* Point to initial location to store parameters in SDRAM */
        sdramBasePtr0 = (Int16 *)SDRAM_BASE_ADDR;
        sdramPtr0 = sdramBasePtr0;
        sdramBasePtr1 = sdramBasePtr0 + SDRAM_LEN/2;
        sdramPtr1 = sdramBasePtr1;
    
        sdram_cntr = 0;
        sdram_flag = 0;
    
        /* Fill memory */
        if (fillMem == TRUE)
        {
            sdram_ptr = (Int16 *)SDRAM_BASE_ADDR;
            for (i=0; i < SDRAM_LEN; i++)
            {
                *sdram_ptr = fillMemVal;
                sdram_ptr++;
            }
        }
    }
    

  • Thanks very much for your feedback, even just a sample project is going to be helpful at the moment. :)