This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CPPI DMA is not working even after all settings!



hi,
I am trying to transmit a packet using CPPI DMA in the response of a HOST. I have done the following initialization and settings in the same sequence, but nothing appears on USB bus, is there any thing i am missing or doing wrong way?
========================
Queue manager control setup
========================
1- Allocate memory for CPPI DMA memory region 0 = 1024*32 Bytes
2- Allocate memory for CPPI DMA link ram 0 = 1024*4 Bytes
3- stored the pointer of Link RAM 0 memory, Link RAM 0 size (1024), and memory region 0 pointer to the related registers
4- Memory region 0 control reg: desc_size= 0 (2^(5+0) = 32), reg_size = 5 (2^(5+5) = 1024), start_index=0 (as only one region is being used)
========================
CPPI control registers setup
========================
5- Tx Channel N Global Configuration Register (using N from 0-14 for 1-15 endpoints) = Just enabled the channels (0-14) by setting the most significant bit in related registers
========================
CPPI Scheduler configuration
========================
6- CPPI DMA Scheduler Table Word N = populated the table up to 8 words (30 entries (15 channels 0-15, each channel has 2 entries in one word that is one for TX and one for RX)). Values are shows as under for these 8 words programmed in this registers
SCHEDULE_WORD0                    0x81018000
SCHEDULE_WORD1                    0x83038202
SCHEDULE_WORD2                    0x85058404
SCHEDULE_WORD3                    0x87078606
SCHEDULE_WORD4                    0x89098808
SCHEDULE_WORD5                    0x8B0B8A0A
SCHEDULE_WORD6                    0x8D0D8C0C
SCHEDULE_WORD7                    0x00008E0E
7- CPPI DMA Scheduler Control Register = Enabled schedular by setting the MSB and also programmed the 30 as number of entries
8- USBSS IRQ_ENABLE_SET = enabled tx_pkt_cmp_0 and rx_pkt_cmp_0 interrupts
=========================
When any endpoint is configured 1st time except EP0
=========================
9- when EP0-EP1 is configured 1st time for usage at that time a 32 bit aligned memory is allocated of 32 bytes for each descriptor for 1024 descriptors (1024 * 32 bytes). This is to store the descriptors we create for this EP.
=========================
While transmitting from a EP except 0 using CPPI DMA
=========================
10- Clear Global RNDIS bit using USB0CTRL register
11- Set requested EP DMA Transparent mode using USB0TXMODE register
12- Required number of descriptors (1 PD and all others BD) are created and filled according to the following, each descriptor is 32 bytes log (8 words).
word0 :: Descriptor type=16, Protocol-specific valid word count=0, Packet length= total data length to be transferred (for BD this reg is written as 0 on all bits)
word1 :: Written the full register with 0
word2 :: type of this packet = 5, On-chip=0, Packet return queue # = set accordingly, (for BD type of this packet is not present )
word3 :: Buffer 0 length = current data length to be transferred in this packet
word4 :: Buffer 0 pointer = address of memory where data to be transmitted is placed
word5 :: Next descriptor pointer = pointer to next descripter
word6 :: Original buffer 0 length = same as Buffer 0 length
word7 :: Original buffer 0 pointer = same as Buffer 0 pointer
13- Pushed all of above created descriptors (PD 1st then other BDs in the sequence) on by one by writing "Queue N Register D" using corresponding Queue number of USB0 Tx Endpoint x (x is 1-15), using the 1st queue of all these 15
-a- desc_ptr = the PD memory address (remember it is 32 bit aligned so last 5 bits will be zero so assuming that controller will append these 5 zeros to make it complete address)
-b- desc_size = 2 ( as descriptor size is 32, so 0=24, 1=28, 2=32, -----)
14- To Enable DMA need to set these 2 things in CSR: -a- Clear Autoset -b- Set DMAReqEnab & DMAReqMode
Waiting for the response. Thank you in advance.
  • Hi,

    TX is working. there was a hidden bit that was marked as Reserved (31st bit of Original Buffer length word of descriptor) and setting this interrupts started appearing and TX is working fine now.

    BUT!

    RX is not working. It remains queued in the queue but not going for processing. Instead rx_sop_starvation interrupt occurs continuously.

    Please help me in this regard. Settings are as following. If there is anything missing or wrong please let me know asap. 

    =====

    -->1st 4 are same as in above post

    ========================
    CPPI control registers setup
    ========================
    5- Rx Channel N Global Configuration Register (using N from 0-14 for 1-15 endpoints) = Enabled the channels (0-14) by setting the most significant bit in related registers AND set the 12 LSB bits to give the Free Descriptor Queues (0-14 for 1-15 endpoints) as receive submission queues.
    --> Next up 9 are same as in above post

    =========================
    While transmitting from a EP except 0 using CPPI DMA
    =========================
    10- Clear Global RNDIS bit using USB0CTRL register
    11- Set requested EP DMA Transparent mode using USB0TXMODE register
    12- Required number of descriptors (1 PD and all others BD) are created and filled according to the following, each descriptor is 32 bytes log (8 words).
    word0 :: Descriptor type=16, Protocol-specific valid word count=0, Packet length= total data length to be transferred (for BD this reg is written as 0 on all bits)
    word1 :: Written the full register with 0
    word2 :: type of this packet = 5, On-chip=0, Packet return queue # = set accordingly, (for BD type of this packet is not present )
    word3 :: Buffer 0 length = current data length to be transferred in this packet
    word4 :: Buffer 0 pointer = address of memory where data to be transmitted is placed
    word5 :: Next descriptor pointer = pointer to next descripter
    word6 :: Original buffer 0 length = same as Buffer 0 length (31st bit set to 1)
    word7 :: Original buffer 0 pointer = same as Buffer 0 pointer
    13- Pushed all of above created descriptors (PD 1st then other BDs in the sequence) one by one by writing "Queue N Register D" using corresponding Queue number(0-14) of USB0 Rx Endpoint x (x is 1-15), i am pushing for EP2 in Free Descriptor Buffer 1
    -a- desc_ptr = the PD memory address (remember it is 32 bit aligned so last 5 bits will be zero so assuming that controller will append these 5 zeros to make it complete address)
    -b- desc_size = 2 ( as descriptor size is 32, so 0=24, 1=28, 2=32, -----)
    14- To Enable DMA used these settings in CSR: -a- Clear Autoset=0 -b- AUTOCLEAR = 1, DMAEN=1 & DMAMODE = 0

    Waiting for the response. Thank you in advance.