This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How do I get WiFi and Bluetooth dongle running on am3517 and Android Gingerbread

Hi,

I have tried all sorts of guides for porting wifi and bluetooth but none seemed to work.

I actually don't think that it could be that difficult, but something clearly is not working right.

The build is ok but when I want to run it from the board, it doesn't work.

Board: TAM3517 Twister Board

Kernel: Linux-2.6.37

OS: Android Gingerbread 2.3.4

Has anyone got any advice on how I could solve this problem?

This is the boot message (only with bluetooth)

0081.boot.txt

thanks in advance

Dominic