hi,
i'm using AM335x with PSP 04.06.00.07, i need a high speed GPIO_1 module so that i can trigger the GPIO1 output (on and off) in 4Mhz, and can detect a input signal (logic level high) which is also 4Mhz.
the original setting of CORE_CLKOUTM4 clock source is 200Mhz divide by 10, so the GPIO_1 module have 20Mhz. But i failed to trigger the output in 4Mhz and failed to detect 4Mhz input signal. Normally the module clock need 10 times bigger than output or input signal, i think i need the GPIO_1 module to have 40Mhz.
How i configure the GPIO_1 module interface clock to have 40Mhz clock?
Thanks & regards
Keldy