This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't access CNTFRQ register

Other Parts Discussed in Thread: AM3359

Hi,

      I'm having issues with the DTIMER interrupt not occurring as frequently as it should. The DMTIMER examples look like the ISR should be occuring approx every .7 seconds but it is more like 2-3 seconds. I wrote a piece of assembly to read the CNTFRQ register as documented on page 1532 of the ARM® Architecture Reference Manual:

To access CNTFRQ, software reads or writes the CP15 registers with <opc1> set to 0, <CRn> set to c14, <CRm> set to
c0, and <opc2> set to 0. For example:
MRC p15, 0, <Rt>, c14, c0, 0 ; Read CNTFRQ into Rt

So when I try to execute the instruction below I end up at an abort vector even though the ARM is executing in Supervisor mode:

MRC             P15, #0, R0, C14, C0, #0

Error:

00000000 ANDEQ           R0, R0, R0
4030fc00:   E59FF018 LDR             PC, 0x4030FC20
4030fc04:   E59FF018 LDR             PC, 0x4030FC24   <-----------------End up here
4030fc08:   E59FF018 LDR             PC, 0x4030FC28
4030fc0c:   E59FF018 LDR             PC, 0x4030FC2C
4030fc10:   E59FF014 LDR             PC, 0x4030FC2C
4030fc14:   E24FF008 SUB             PC, PC, #8
4030fc18:   E59FF010 LDR             PC, 0x4030FC30
4030fc1c:   E59FF010 LDR             PC, 0x4030FC34

Does StarterWare have any examples of trying to read the CNTFRQ register so I can verify the system clock frequency?

Thanks....

  • Hi John,

    The CNTFRQ register is part of system timer, and this is not part of Cortex-A8 core I think. So, that operation is invalid.

    And, coming to the actual problem that, in the DMTimer example the ISR is triggered every 2-3 seconds instead of .7 seconds,

    Have you done any modification to the existing example ? which platform are you testing ?

    Regards,

    Sujith.

  • Hi Sujith,

                    The CNTFRQ is actually part of the Cortex-A8 and should be accessible as long as your are running in supervisor mode (is there something different about getting to the register in the AM3359?). We are using the Critical Link MityArm development board which also uses a 24M oscillator (same as Beaglebone.) We allow the Linux Uboot to bring up the card and then load StarterWare instead of the kernel. I have not changed any of the DMTimer programming (it is using the CLK_M_OSC for the timers.) I just trying to verify what the ARM actually thinks is the system frequency is, hence trying to look at the CNTFRQ register. The DMTimer examples use an up count of 0xffffff before a rollover is supposed to trigger the isr:

      0xffffff = 16, 777, 215 ==> 1/24Mhz * 16, 777, 215 = .698938 seconds ~ .7 seconds

    Is there some other way to try to verify the AM3359 DMTimers clocking?

    Thanks,

         John C.

  • Hi John,

    I dont see the Generic Timer (and hence CNTFRQ register) in Cortex-A8 TRM. May be the difference lies between StarterWare bootloader and the one you are using in some PLL configs.. You can probably check for the same. I think there is no pin-out  of Timer input clock.

    Regards,

    Sujith.

  • Hi Sujith,

                   I will admit that you will not find mention of the register in the TRM, but the ARM (Architecture Reference Manual) for the ARMv7-A and ARMv7-R does mention it, so I assume that it is in the core. The u-boot code uses the same type of assembly instruction to access the CSSELR (Cache Size Selection Register) which is another register not in the TRM.

        /* Write to Cache Size Selection Register(CSSELR) */
        asm volatile ("mcr p15, 2, %0, c0, c0, 0" : : "r" (csselr));

         This clip of code was from a u-boot file cache_v7.c written by Aneesh V at TI. All of these registers seem to revolve around the p15 reference in the assembly, but even in Arch. reference manual they never have a summarized list of what is available. According to manual the CNTFRQ is supposed to be programmed early on in boot. Is the source code available for the StarterWare bootloader on the beaglebone ?

    Thanks,

         John C.




  • Hi John,

    The source code is definitely available for StarterWare bootloader. You can refer the files in "/bootloader/src/" folder.

    And, to add to CNTFRQ related query:

    You are right that it is mentioned in ARM ARMv7 A and R document. But Cortex-A8 is an implementation of ARMv7a which doesn't include a Generic Timer. But Cortex-A15 is another implementation of the same version, which includes the Generic Timer. Everything described in ARMv7A and R document may not be part of the particular implementation. Hope now its clear. :)

    And, the CSSELR is a part of Cortex-A8 and is present in the datasheet as well

    Cheers,

    Sujith.

  • Sujith,

             Well that would explain why the processor aborts. It has definable been a frustrating part of working with the ARM processors in that the ARM documents don't have something like a summary table that shows which Cortex variations have which components. The ARM document does not even have the word Cortex in it. The Cortex-A8 link below will lead you to the Architecture document that I have been using.

    http://www.arm.com/products/processors/cortex-a/cortex-a8.php

    Can you tell me where you found out that the A8 does not have the generic timer? If it is not in the A8, then the Architecture document should at least have some mention of reference another document about specific implementations.

    Thanks,

         John Conover

  • Hi John,

    I dont know whether anywhere it is mentioned that "Generic timer is not part of Cortex-A8". But what I see normally is, the TRM of a particular implementation contains the features supported by that core. This may not be in detail. For the details, we need to refer to the corresponding architecture version's ARM Architecture Reference Manual.

    Regards,

    Sujith.