Other Parts Discussed in Thread: TMS320C5505, TMS320C5515
Hi,
I am working on c5505 DSP , and I am trying to boot using SPI flash.
However, when I try to use the programmer with my "file.out" (built with Hex55.exe), it gives me an error :
WRITE ERROR at 0x0000
I am using the SST25VF032B SPI Serial Flash. So I wanted to know if it is
Compatible with the TMS320C5505 DSP, and, if it is, what could be the cause of this issue.
I tried with two different programmers I found on this forum:
The programmer_C5515_EVM.out, and the one I found in the evm5505_v1 folder, but I experienced the same issue with both.
Does anyone have a suggestion why I would be getting this error?
Regards,
Antoine