This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM37xx: Software Booting Configuration (TRM chapter 26.4.4)



Hi,

 

a customer is having a hard time getting the warm reset to work properly. The customer is trying to get a boot-order via Software booting configuration of MMC1, MMC2

After a warm reset the processor always boots off of MMC2. The sys_boot pins are set to 5:0 ( 110001). This gives a cold reset sequence of USB, UART3, MMC1, MMC2 (Table 26-4) and a warm reset of MMC2 only (Table 26-5).

However, as per section 26.4.4.3 of SPRUGN document, this order can be changed using the scratch pad memory (see Figure 26-9) which overrides the sys_boot pins. We have written scratch pad memory located at address 0x48002910 to (refer to section 26.4.4.4 and Table 26-12)

Here are a few trials to write that internal memory:

 

___address____|_0__1__2__3__4__5__6__7__01234567

  NSD:48002910|01 AA 00 CF 0C 00 00 00 ........

  NSD:48002918| 1E 00 06 00 00 00 05 00 ........

  NSD:48002920| 00 00 00 00 00 00 00 00 ........

  NSD:48002928| 00 00 00 00 00 00 00 00 ........

  NSD:48002930| 00 00 00 00 00 00 00 00 ........

  NSD:48002938| 00 00 00 00 00 00 00 00 ........

  NSD:48002940| 00 00 00 00 00 00 00 00 ........

  NSD:48002948| 00 00 00 00 00 00 00 00 ........

 

 

___address____|_0__1__2__3__4__5__6__7__01234567

  NSD:48002910|01 AA 00 CF 0C 00 00 00 ........

  NSD:48002918| 00 1E 00 06 00 05 00 00 ........

  NSD:48002920| 00 00 00 00 00 00 00 00 ........

  NSD:48002928| 00 00 00 00 00 00 00 00 ........

  NSD:48002930| 00 00 00 00 00 00 00 00 ........

  NSD:48002938| 00 00 00 00 00 00 00 00 ........

  NSD:48002940| 00 00 00 00 00 00 00 00 ........

  NSD:48002948| 00 00 00 00 00 00 00 00 ........

 

___address____|_0__1__2__3__4__5__6__7__01234567

  NSD:48002910|CF 00 AA 01 00 00 00 0C ........

  NSD:48002918| 00 1E 00 06 00 05 00 00 ........

  NSD:48002920| 00 00 00 00 00 00 00 00 ........

  NSD:48002928| 00 00 00 00 00 00 00 00 ........

  NSD:48002930| 00 00 00 00 00 00 00 00 ........

  NSD:48002938| 00 00 00 00 00 00 00 00 ........

  NSD:48002940| 00 00 00 00 00 00 00 00 ........

  NSD:48002948| 00 00 00 00 00 00 00 00 ........

 

Somehow it is still not working. Are there working examples of writing the Software Boot Configuration memory locations?

 

 

Thanks,

--Gunter 

 

 

 

 

 

  • Hi all,

     

    could you provide an update on this issue??

     

    Thanks,

    --Gunter

  • In reading the TRM it looks like the word at 0x48002910 is a pointer to that structure in memory.

    0x48002910: 14 29 00 48

    0x48002914: 01 AA 00 CF

    etc.

     

  • Hi all,

     

    still trying to find the right format

     

    To summarize

    Using TRM Table 13-75 for CONTROL_SAVE_RESTORE_MEM

    Wake-Up Booting by ROM Code

    In CORE OFF power state, all configurations outside the WKUP power domain are reset and must be

    restored to restart the system in the condition it was in before being stopped. After an MPU and CORE

    power domain wake-up reset, the ROM code restores the SDRC and clock settings to allow a jump to a

    public restore function. This public restore function is specifically implemented by users to restore their

    own hardware and software environments. Users must set the public restore function address in the public

    restore pointer field of the CONTROL_SAVE_RESTORE_MEM structure.

    The CONTROL_SAVE_RESTORE_MEM memory of the SCM saves and restores mandatory information

    to automatically reconfigure the SDRC and PRCM registers. The SDRC and clock registers must be

    saved by users in the respective structures (see Table 26-50 and Table 26-51) in the SCM (scratchpad

    memory) before going to off mode to be automatically restored on wake-up boot by the ROM code.

    The size of CONTROL_SAVE_RESTORE_MEM is 240 bytes starting at the hardware physical address

    0x48002910 to 0x480029FF. Figure 26-31 shows the memory format that must be obeyed to handle the

    context restoration.

     

    Using Figure 26-31 CONTROL_SAVE_RESTORE_MEM Format

    Using Tables 26-50 and 51

     

    Here is my thought:

    0x48002910  Pointer to Boot Config structure

    0x48002914 … 0x480029C0 PRCM registers save, SDRC registers save – Let’s not touch this area!

    0x480029C0 … 0x480029FF Area for Actual booting configuration structure

     

     

    So I am thinking to put the boot config structure in as follows:

    0x48002910   C0 29 00 48

    0x480029C0   01 AA 00 CF

    (use what you had before)

     

    Do you agree with this?

    Now I need to look at the right boot config structure itself.

     

     

    Thanks,

    --Gunter

  • Hi all,

     

    With the above in mind, our first test will be

     

    0x48002910         C0 29 00 48          pointer to boot config

     

    Boot config

    0x480029C0        01 AA 00 CF         sync key for section 1

    0x480029C4        0C 00 00 00          size of section 1

    0x480029C8        1E 00 06 00          disable all CH, first boot device MMC1

    0x480029CC        05 00 06 00          second boot device MMC2, third boot device MMC1

    0x480029E0         05 00 00 00          fourth boot device MMC2, 2 bytes of padding

    No further sections

     

    This is using TRM Table 26-12.

     

    Please comment if anyone has tried this.

     

    Thanks,

    --Gunter

     

  • Gunter,

    Have you tried setting all of them to MMC1(given below) or UART boot? This will give a clear idea whether its really picking your custom settings or not. 

    0x480029C0        01 AA 00 CF

    0x480029C4        0C 00 00 00

    0x480029C8        1E 00 06 00          

    0x480029CC        06 00 06 00          

    0x480029E0         06 00 00 00

    How are you writing and reading the scratch pad memory?

  • Hi Renjith,

     

    we have sucessfully used the following scratchpad memory for software boot configuration. This worked:

     

    0x48002910         C0 29 00 48          pointer to boot config

     

    Boot config

    0x480029C0        01 AA 00 CF         sync key for section 1

    0x480029C4        0C 00 00 00          size of section 1

    0x480029C8        1E 00 06 00          disable all CH, first boot device MMC1

    0x480029CC        05 00 06 00          second boot device MMC2, third boot device MMC1

    0x480029E0         05 00 00 00          fourth boot device MMC2, 2 bytes of padding

     

    We are assuming the memory allocations from the TRM and have tried not to overwrite anything.

     

    Regards,

    --Gunter