Other Parts Discussed in Thread: TVP7002
Hello,
I need to capture and process simultaneous videos for stereo vision. One of my friend claimed that, the baseboard of this evolution module has no video input and Expansion I/O Daughter card has only one component input, one VGA input and one HDMI input. I just wonder that is it possible to connect two same model camera to DM816x Development Board with two same connector type ? For example is it possible to connect two USB cameras via USB ports on board or two GigE cameras via ethernet ports?