This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 EZSDK Some problem about PCIE when booting kernel

I use the linux-2.6.37-psp04.04.00.01.

U-Boot 2010.06 (Mar 01 2013 - 16:07:59)

TI8168-GP rev 1.1

ARM clk: 987MHz
DDR clk: 398MHz

I2C:   ready
DRAM:  1 GiB
NAND:  ======================================================
mtd->writesize, mtd->oobsize , mtd->erasesize = 2048,64,131072
256 MiB
Net:   Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot:  0
UBOOT11 #
UBOOT11 #
UBOOT11 # bootm 0x81000000
## Booting kernel from Legacy Image at 81000000 ...
   Image Name:   Linux-2.6.37
   Created:      2012-10-12   8:18:23 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2594212 Bytes = 2.5 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (user@ubuntu.workshop.net) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #23 Fri Oct 12 00:37:57 PDT 2012
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
bootconsole [earlycon0] enabled
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 1.1
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 52224
Kernel command line: console=ttyO2,115200n8 rootwait rw mem=256M root=/dev/nfs nfsroot=192.168.1.48:/home/song/targetfs ip=192.168.1.21:192.168.1.43:192.168.1.43:255.255.255.0::eth0:off notifyk.vpssm3_sva=0xBF900000 earlyprintk
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 206MB = 206MB total
Memory: 203108k/203108k available, 59036k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
    vmalloc : 0xd0800000 - 0xf8000000   ( 632 MB)
    lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .init : 0xc0008000 - 0xc003c000   ( 208 kB)
      .text : 0xc003c000 - 0xc04e7000   (4780 kB)
      .data : 0xc04e8000 - 0xc0531200   ( 293 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
_omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
_omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS
registered ti816x_gpio_vr device
registered ti816x_sr device
pm_dbg_init: only OMAP3 supported
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd0820000

The boot kernel stopped here and can not read the  PCIESS Application Registers etc. 

Can someone from TI explain what is going wrong?

Thanks,
Wu