Hi,
I want to set the PINMUX registers in the OnTargetConnect() function in GEL, what confused is that if i set the PINMUX15 register, then every time when i connect the target, an error present: "GEL: Error while executing OnTargetConnect(): cannot multiply by pointer". And the other PINMUX registers seems OK, as long as i do not set the PINMUX15.
Any one encountered the same problem?
Thanks,
Huang.