what's this error????
Sending DHCP requests ...... timed out!
IP-Config: Retrying forever (NFS root)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what's this error????
Sending DHCP requests ...... timed out!
IP-Config: Retrying forever (NFS root)
Not sure abt the entire setup of your environment, but see if this post helps you.
mostafa safaie said:what's this error????
Sending DHCP requests ...... timed out!
IP-Config: Retrying forever (NFS root)
IP-Config: or Internet Protocol Configuration. Getting requests timed out means it is not getting an answer back to it with the type of network connection it thinks it should use. You did say you checked your connections, did you check how it thinks it should connect? There has been more than one time I have switched either to or from wireless and forgot to set as such that caused similar issues. Also with connecting with wireless, I have had issues with trying to connect and at a mid level check, found that the error was not settings, not the router, not the wireless, it was the neighbor's router was showing up as a strong signal and since I don't have access to their network, could not connect.
What type of connection are you using and if it is cable, can you swap to known good cables?
Eric
you're right.
I'm using wireless connection but I can't set it.....
what must do???
what device are you using to connect and what wireless technology are you setting up for the wireless connection on the device side?
What 802 standard ( wireless type ) does your router support?