Dear all,
I upgrade firmware Ver 3.1 for platform DM36x+SONY IMX036 sensor, with the firmware and its name as below for the kernel and root file system.
uImage_ipnc_dm368_IMGS_SONY_IMX036_3MP_3.0
ipnc_dm368_IMGS_SONY_IMX036_3MP_3.0.squashfs
As a result the snap shot happen to an error while the video stream is in 3M H264 .
The error message is like..
[ 218.420000] CMEMK Error: ioctl: failed to allocate heap buffer of size 0x300000
CMEM Error: allocHeap: ioctl CMEM_IOCALLOCHEAP failed: -1
ERROR (alg_jpgEnc.c|SnapshotFrameData|275): XDM1_BufDesc failed
Does anyone happen to the same situation?
Has any idea? to fix it