This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c674x dsplib padding



Hi All,

I'm using c674x dsplib 3.1.0.0 for fft/ifft, functions DSPF_sp_ifftSPxSP/DSPF_sp_fftSPxSP.

I noticed that the demo code (DSPF_sp_fftSPxSP_d.c) does use some padding both at the beginning and at the end of x/y/w arrays.

However, neither the code nor the documentation of c674x dsplib mentions that it'd be necessary to add padding.

I took a look of C67x dsplib, and there the doc says (http://www.ti.com/lit/ug/spru657c/spru657c.pdf) that for DSPF_sp_ifftSPxSP input array x needs a padding at the end.

So I'd like to ask, if in case of c674x dsplib DSPF_sp_ifftSPxSP/DSPF_sp_fftSPxSP do one need to add some padding, if yes, then for which arrays, how long and at the beginning and/or at the end?

Thanks,

Istvan