This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMA memory map for tomahawk c6486 ???

Hey hi all,
I am  building the dimtesthd on linux host machine for Tomahawk 6486.... I have built it and then loaded an application it was successful..
But while looking the source code of dimtesthd i am not able to understand some addresses which are used in /vng/common/micro/dim/dimloc.h...... if anybody know about this then please let me know..   also whats the DMA memory map for tomahawk...???



  #define DIM_C6486_START_VECTOR              0x00800000  /* In bytes */                                       

 293 #define DIM_C6486_LOCAL_MEM_START1          0x00400000  /* in words */

 295 #define DIM_C6486_LOCAL_MEM_END1            0x0044C000  /* in words */

 297 #define DIM_C6486_LOCAL_MEM_START2          0x00700000  /* in words */

 299 #define DIM_C6486_LOCAL_MEM_END2            0x00704000  /* in words */

 301 #define DIM_C6486_LOCAL_MEM_START3          0x00780000

 303 #define DIM_C6486_LOCAL_MEM_END3            0x00784000  /* in words */

    what are these addresses and from where these are taken... ????

regards

Ashwini