Other Parts Discussed in Thread: OMAP-L138
Hi,
I am working on TI's OMAP L138/C6748 Development kit (LCDK) with XDS510 USB PLUs and CCSv5. Also I have installed MAPL138_StarterWare_1_10_03_0 on my PC.
I can build and run some sample code on the development board without problem that make me think the my configuration is OK. However when I ran McASP example code under /lcdkOMAPL138/ fonder it seems it crashed on the board with a message 'system in reset'. After this I have to disconnect and power off/on to recover. I am just wondering anyone here had similar experience with LCDK board?. Thanks.
Yan