Hi, guys. I know that the BM is calculated by DSP, and I'm wondering that if the BM is calculated in advance before decoding by VCP or the BM can be calculated while do decoding by VCP at the same time?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, guys. I know that the BM is calculated by DSP, and I'm wondering that if the BM is calculated in advance before decoding by VCP or the BM can be calculated while do decoding by VCP at the same time?
Hi Yang,
as the branch metrics are an input to the VCP2 you need to calculate before sending of to the VCP2.
But since the VCP2 is operating independently from the CPU you can calculate the BM in parallel with the VCP2. This means you can implement a pipelining scheme to continuously feed the VCP2.
Kind regards,
one and zero
Hi one and zero,
Thanks for the response. I believe that while it may be possible to implement a pipeline as you suggested (since VCP2 does not need all the BM data at once before it can start decoding), this can cause a race condition. BM data is transferred to the VCP2 using EDMA which would be a lot faster than the rate at which the DSP (software) can write BM data to the input buffer in which case VCP2 can end up reading junk data from the BM input buffer.
I believe its a safer strategy to calculate and store the BM data in the input buffer before decoding is started. Kindly comment if I missed something. Thanks.
Regards
-Nitin