This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 Mpeg2 encoder compliance problem.



Hi,

Im using DVSDK 4.0.2, dm365 evm and mpeg2 encoder to perform create a DVB-S stream. A DVB-S stream requires a valid compliant mpeg2 stream ( later muxed to be TS). However using the ffmpeg mpeg2 encoder I was able to create a stream which was complaint (with further processing my own stuff) however with dm365 and dvsdk demos mpeg2 encoder I was not.

I decided to create two files with each encoder and analyze then on where the problem lies and I will post some images. It turns out that ffmpeg's mpeg2 encoder repeats frames of SEQUNCE - SEQUENCE EXTENSION - GOP , Every 14 frames as required by the MPEG 2 standard but dm365's mpeg2 encoder does not

Image showing sequence frames of ffmpeg mpeg2: http://postimage.org/image/f8si5u0wz/

Image Showing sequence frames of dm365 mpeg2: http://postimage.org/image/h8ay2soh1/

You can clearly see the differences between the streams. The analyzer also reports 55 (Fair) for dm365 stream and 80 (Excellent) for ffmpeg streams (should not make a difference but this is how the analyzer ranks it in terms of compliance).

Is there a reason for this implementation? , Is there a solution to this problem?

Thanks for your help.

Regards,

Sam

  • Sorry for delayed response - below is what i managed to gather - 

    If it is looking for Intra frames and sequence headers every 15 frames then following solution will help

    1. Send generate header for every 15 calls. This can be done by dynParams->videncDynamicParams.generateHeader.
    2. Setting intraFrameInterval to 15. This is also part of dynParams.
    Regards
    Yashwant
  • Hi Yashwant,

    Thanks for your response, the problem is the missing GOP structures within the stream. It is actually discussed here in a thread http://e2e.ti.com/support/embedded/multimedia_software_codecs/f/356/t/42309.aspx. The solution you mentioned above will generate seq headers but what of the GOP structure which would still be missing?. Any way around that?

    Best Regards,

    Samer Tufail

  • We dont have B frame support in DM365 mpeg2 encoder.

     

    regards

    Yashwant