This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Capturetest application giving exception when preview enabled.

Hi,

we are working on capturetest application. 

Following is the configuration

- wince 6.0

- dvsdk_wince_1_00_00_05

- omap 3530

Platform - EVM DM3730

 

if we are runing CaptureTest app without preview it is working fine.

But If Capturetest application running with preview enabled, giving exception as below

Exception 'Data Abort' (4): Thread-Id=07f50012(pth=8f7c1120), Proc-Id=0218007a(pprc=8c467eac) 'capturetest.exe', VM-active=0218007a(pprc=8c467eac) 'capturetest.exe'
PC=4140b144(quartz.dll+0x000bb144) RA=00000000(???+0x00000000) SP=0052fce8, BVA=001b9000

 when we changed the focus of render window then this is happening.

Why this Exception is coming? Can any one help me to resolve the issue?

 

Thanks,