Other Parts Discussed in Thread: SYSBIOS
Hi,
I am trying to use zero latency interrupt for EPWM1_INT interrupt. Since this interrupt is located in PIE Group 3 I used the following settings in .cfg file
var Hwi = xdc.useModule('ti.sysbios.family.c28.Hwi');
Hwi.zeroLatencyIERMask = 0x0004;
I added following lines in main function before BIOS_start().
Hwi_plug(48,OffsetISR);
Hwi_enablePIEIER(3,0x0001);
Following lines are added at the end of the OffsetISR function
PieCtrlRegs.PIEACK.bit.ACK3 = 1; // Acknowledge interrupt to PIE
The code compiles without an error or warning. I run it on ezDsp28335 board PIE registers are
PIEIER3= 0x0001
PIEIFR3= 0x0001
However, the interrupt register in the core
IER.INT3 is zero in other words it seems INT3 is not activated.
I installed bios_setupwin32_6_34_01_14.exe but it does not help.
Can somebody send an example code for implementation of zero latency interrupts?
Regards,
Burak Kelleci