This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bluetooth: st_register failed -22

Other Parts Discussed in Thread: TMDXEVM3358, WL1271, TPS65910, DA8XX, TMP275

Hi all.

My board is TMDXEVM3358. Also it contains WL1271 module for Wi-Fi and Bluetooth.

In my test yesterday, i was able to send files from Bluetooth with OPP. It worked good. Almost 2 days worked good.

But suddenly, Bluetooth stopped to working. It's impossible to enable from UI (Settings menu) When i turn it on, it turn off automaticly.

Also i noticed that, on debug termina there are 2 errors came periodicly.

[ 443.062927] (stk) :line disc installation timed out
[ 445.182922] (stk) :line disc installation timed out
[ 447.302917] (stk) :line disc installation timed out
[ 449.422912] (stk) :line disc installation timed out
[ 451.542938] (stk) :line disc installation timed out
[ 452.542938] Bluetooth: st_register failed -22
[ 453.762908] (stk) :line disc installation timed out
[ 455.882934] (stk) :line disc installation timed out
[ 458.002929] (stk) :line disc installation timed out
[ 460.122924] (stk) :line disc installation timed out
[ 462.242919] (stk) :line disc installation timed out
[ 464.362915] (stk) :line disc installation timed out
[ 465.362945] Bluetooth: st_register failed -22

Any idea?

Note: Wi-Fi side is working.

  • 1. If possible, can you try a previously working image to verify that this is not a hardware issue.

    2. Could you attach the full logs?

  • I work with NAND image. And i tried NAND and SD-Card Image(TI Kit provided) but same.

    Debug logs;

    U-Boot SPL 2011.09-00000-g518a597 (Apr 11 2012 - 16:55:25)
    Texas Instruments Revision detection unimplemented
    OMAP SD/MMC: 0
    reading u-boot.img
    reading u-boot.img


    U-Boot 2011.09-00000-g518a597 (Apr 11 2012 - 16:55:25)

    I2C: ready
    DRAM: 256 MiB
    WARNING: Caches not enabled
    Found a daughter card connected
    NAND: HW ECC Hamming Code selected
    256 MiB
    MMC: OMAP SD/MMC: 0
    *** Warning - bad CRC, using default environment

    Net: cpsw
    Hit any key to stop autoboot: 0
    SD/MMC found on device 0
    reading uEnv.txt

    214 bytes read
    Loaded environment from uEnv.txt
    Importing environment from mmc ...
    Running uenvcmd ...
    reading uImage

    3574432 bytes read
    ## Booting kernel from Legacy Image at 82000000 ...
    Image Name: Linux-3.2.0-gb02ab39
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 3574368 Bytes = 3.4 MiB
    Load Address: 80008000
    Entry Point: 80008000
    Verifying Checksum ... OK
    Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    [ 0.000000] Linux version 3.2.0-gb02ab39 (x0029463@psplinux052) (gcc version
    4.4.3 (GCC) ) #1 Wed Apr 11 14:03:37 IST 2012
    [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
    [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
    n cache
    [ 0.000000] Machine: am335xevm
    [ 0.000000] Memory policy: ECC disabled, Data cache writeback
    [ 0.000000] AM335X ES1.0 (sgx neon )
    [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pag
    es: 65024
    [ 0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=t
    tyO0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off
    [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [ 0.000000] Memory: 256MB = 256MB total
    [ 0.000000] Memory: 251520k/251520k available, 10624k reserved, 0K highmem
    [ 0.000000] Virtual kernel memory layout:
    [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
    [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
    [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
    [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
    [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
    [ 0.000000] .text : 0xc0008000 - 0xc0660000 (6496 kB)
    [ 0.000000] .init : 0xc0660000 - 0xc069b000 ( 236 kB)
    [ 0.000000] .data : 0xc069c000 - 0xc06f40e0 ( 353 kB)
    [ 0.000000] .bss : 0xc06f4104 - 0xc0823888 (1214 kB)
    [ 0.000000] NR_IRQS:396
    [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrup
    ts
    [ 0.000000] Total of 128 interrupts on 1 active controller
    [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
    [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
    [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 13
    1071999ms
    [ 0.000000] Console: colour dummy device 80x30
    [ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
    [ 0.058929] pid_max: default: 32768 minimum: 301
    [ 0.059051] Security Framework initialized
    [ 0.059143] Mount-cache hash table entries: 512
    [ 0.059509] CPU: Testing write buffer coherency: ok
    [ 0.079498] omap_hwmod: gfx: failed to hardreset
    [ 0.095764] omap_hwmod: pruss: failed to hardreset
    [ 0.096557] print_constraints: dummy:
    [ 0.096771] NET: Registered protocol family 16
    [ 0.097839] OMAP GPIO hardware version 0.1
    [ 0.098876] omap_mux_init: Add partition: #1: core, flags: 0
    [ 0.100189] omap_i2c.1: alias fck already exists
    [ 0.100677] omap2_mcspi.1: alias fck already exists
    [ 0.100799] omap2_mcspi.2: alias fck already exists
    [ 0.100952] edma.0: alias fck already exists
    [ 0.100952] edma.0: alias fck already exists
    [ 0.100982] edma.0: alias fck already exists
    [ 0.109680] bio: create slab <bio-0> at 0
    [ 0.110626] SCSI subsystem initialized
    [ 0.111450] usbcore: registered new interface driver usbfs
    [ 0.111572] usbcore: registered new interface driver hub
    [ 0.111724] usbcore: registered new device driver usb
    [ 0.111846] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
    [ 0.111999] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
    [ 0.128997] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
    [ 0.130249] tps65910 1-002d: JTAGREVNUM 0x0
    [ 0.132415] print_constraints: VRTC:
    [ 0.133758] print_constraints: VIO: at 1800 mV
    [ 0.135986] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
    [ 0.138214] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
    [ 0.139099] print_constraints: VDD3: 5000 mV
    [ 0.140411] print_constraints: VDIG1: at 1800 mV
    [ 0.141754] print_constraints: VDIG2: at 1800 mV
    [ 0.143096] print_constraints: VPLL: at 1800 mV
    [ 0.144409] print_constraints: VDAC: at 1800 mV
    [ 0.145751] print_constraints: VAUX1: at 1800 mV
    [ 0.147064] print_constraints: VAUX2: at 3300 mV
    [ 0.148406] print_constraints: VAUX33: at 3300 mV
    [ 0.149719] print_constraints: VMMC: at 3300 mV
    [ 0.150024] tps65910 1-002d: No interrupt support, no core IRQ
    [ 0.150390] Advanced Linux Sound Architecture Driver Version 1.0.24.
    [ 0.150970] Bluetooth: Core ver 2.16
    [ 0.151031] NET: Registered protocol family 31
    [ 0.151031] Bluetooth: HCI device and connection manager initialized
    [ 0.151062] Bluetooth: HCI socket layer initialized
    [ 0.151062] Bluetooth: L2CAP socket layer initialized
    [ 0.151123] Bluetooth: SCO socket layer initialized
    [ 0.151306] Switching to clocksource gp timer
    [ 0.158935] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
    [ 0.159210] musb-hdrc musb-hdrc.0: dma type: pio
    [ 0.159820] musb-hdrc musb-hdrc.0: USB OTG mode controller at d081c000 using
    PIO, IRQ 18
    [ 0.160095] musb-hdrc musb-hdrc.1: dma type: pio
    [ 0.160339] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    [ 0.160400] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
    r 1
    [ 0.160552] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [ 0.160583] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
    1
    [ 0.160583] usb usb1: Product: MUSB HDRC host driver
    [ 0.160614] usb usb1: Manufacturer: Linux 3.2.0-gb02ab39 musb-hcd
    [ 0.160614] usb usb1: SerialNumber: musb-hdrc.1
    [ 0.161102] hub 1-0:1.0: USB hub found
    [ 0.161132] hub 1-0:1.0: 1 port detected
    [ 0.161590] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using
    PIO, IRQ 19
    [ 0.161956] NET: Registered protocol family 2
    [ 0.162170] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.162536] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    [ 0.162689] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
    [ 0.162780] TCP: Hash tables configured (established 8192 bind 8192)
    [ 0.162811] TCP reno registered
    [ 0.162811] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.162841] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.163024] NET: Registered protocol family 1
    [ 0.163330] RPC: Registered named UNIX socket transport module.
    [ 0.163330] RPC: Registered udp transport module.
    [ 0.163330] RPC: Registered tcp transport module.
    [ 0.163360] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [ 0.163604] NetWinder Floating Point Emulator V0.97 (double precision)
    [ 0.289855] ashmem: initialized
    [ 0.290130] VFS: Disk quotas dquot_6.5.2
    [ 0.290191] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [ 0.291076] msgmni has been set to 491
    [ 0.292114] io scheduler noop registered
    [ 0.292114] io scheduler deadline registered
    [ 0.292205] io scheduler cfq registered (default)
    [ 0.294708] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
    [ 0.936767] console [ttyO0] enabled
    [ 0.940795] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    [ 0.948486] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    [ 0.956115] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
    [ 0.963775] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
    [ 0.971405] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
    [ 0.985046] brd: module loaded
    [ 0.991271] loop: module loaded
    [ 0.994812] i2c-core: driver [tsl2550] using legacy suspend method
    [ 1.001251] i2c-core: driver [tsl2550] using legacy resume method
    [ 1.007690] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 1.021606] Detected a daughter card on AM335x EVM..
    [ 1.026611] Unknown CPLD version found, falling back to 1.0A
    [ 1.032745] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [ 1.047912] Board name: A33515BB
    [ 1.051269] Board version: 1.4A
    [ 1.054565] SKU: SKU#01
    [ 1.057647] The board is general purpose EVM in profile 0
    [ 1.063293] Found invalid GP EVM revision, falling back to Rev1.1A
    [ 1.070037] da8xx_lcdc.0: alias fck already exists
    [ 1.075622] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
    [ 1.094879] TSC connected to beta GP EVM
    [ 1.099792] omap-gpmc omap-gpmc: GPMC revision 6.0
    [ 1.104858] Registering NAND on CS0
    [ 1.108886] omap_i2c.2: alias fck already exists
    [ 1.131958] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz
    [ 1.138153] tsl2550 2-0039: standard operating mode
    [ 1.144104] tsl2550 2-0039: registering lightsensor-level input device
    [ 1.151153] input: lightsensor-level as /devices/virtual/input/input0
    [ 1.157897] tsl2550 2-0039: support ver. 1.2 enabled
    [ 1.163391] davinci-mcasp.1: alias fck already exists
    [ 1.169067] omap_hsmmc.0: alias fck already exists
    [ 1.174346] omap_hsmmc.2: alias fck already exists
    [ 1.179565] am335xevm: bt init
    [ 1.183715] (stk) :sysfs entries created
    [ 1.187896] (stk) : debugfs entries created
    [ 1.192291] _regulator_get: 2-0018 supply Vdd not found, using dummy regulato
    r
    [ 1.200073] _regulator_get: 2-0018 supply Vdd_IO not found, using dummy regul
    ator
    [ 1.228637] lis3lv02d: 8 bits 3DLH sensor found
    [ 1.322174] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d
    /input/input1
    [ 1.332458] mtdoops: mtd device (mtddev=name/number) must be supplied
    [ 1.339447] omap2-nand driver initializing
    [ 1.344055] ONFI flash detected
    [ 1.347442] ONFI param page 0 valid
    [ 1.351104] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G
    08ABAEAWP)
    [ 1.359893] Creating 8 MTD partitions on "omap2-nand.0":
    [ 1.365478] 0x000000000000-0x000000020000 : "SPL"
    [ 1.371459] 0x000000020000-0x000000040000 : "SPL.backup1"
    [ 1.377960] 0x000000040000-0x000000060000 : "SPL.backup2"
    [ 1.384429] 0x000000060000-0x000000080000 : "SPL.backup3"
    [ 1.390899] 0x000000080000-0x000000260000 : "U-Boot"
    [ 1.397674] 0x000000260000-0x000000280000 : "U-Boot Env"
    [ 1.404083] 0x000000280000-0x000000780000 : "Kernel"
    [ 1.412200] 0x000000780000-0x000010000000 : "File System"
    [ 1.522613] OneNAND driver initializing
    [ 1.527252] CAN device driver interface
    [ 1.531219] CAN bus driver for Bosch D_CAN controller 1.0
    [ 1.581939] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    [ 1.588409] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
    [ 1.595703] davinci_mdio.0: probed
    [ 1.599243] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
    [ 1.606689] PPP generic driver version 2.4.2
    [ 1.611328] PPP BSD Compression module registered
    [ 1.616241] PPP Deflate Compression module registered
    [ 1.621612] usbcore: registered new interface driver cdc_ether
    [ 1.627746] usbcore: registered new interface driver cdc_eem
    [ 1.633728] usbcore: registered new interface driver dm9601
    [ 1.639556] usbcore: registered new interface driver cdc_subset
    [ 1.645782] cdc_ncm: 04-Aug-2011
    [ 1.649200] usbcore: registered new interface driver cdc_ncm
    [ 1.655212] usbcore: registered new interface driver cdc_acm
    [ 1.661102] cdc_acm: USB Abstract Control Model driver for USB modems and ISD
    N adapters
    [ 1.669464] Initializing USB Mass Storage driver...
    [ 1.674682] usbcore: registered new interface driver usb-storage
    [ 1.680938] USB Mass Storage support registered.
    [ 1.685913] usbcore: registered new interface driver usbserial
    [ 1.692047] USB Serial support registered for generic
    [ 1.697357] usbcore: registered new interface driver usbserial_generic
    [ 1.704193] usbserial: USB Serial Driver core
    [ 1.708770] USB Serial support registered for GSM modem (1-port)
    [ 1.715179] usbcore: registered new interface driver option
    [ 1.720977] option: v0.7.2:USB Driver for GSM modems
    [ 1.727966] gadget: Mass Storage Function, version: 2009/09/11
    [ 1.734191] gadget: Number of LUNs=1
    [ 1.738006] lun0: LUN: removable file: (no medium)
    [ 1.743347] gadget: android_usb ready
    [ 1.747283] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    [ 1.752899] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus numbe
    r 2
    [ 1.760711] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    [ 1.767791] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=
    1
    [ 1.775329] usb usb2: Product: MUSB HDRC host driver
    [ 1.780517] usb usb2: Manufacturer: Linux 3.2.0-gb02ab39 musb-hcd
    [ 1.786865] usb usb2: SerialNumber: musb-hdrc.0
    [ 1.792114] hub 2-0:1.0: USB hub found
    [ 1.796051] hub 2-0:1.0: 1 port detected
    [ 1.800750] mousedev: PS/2 mouse device common for all mice
    [ 1.807434] input: matrix-keypad as /devices/platform/matrix-keypad/input/inp
    ut2
    [ 1.816192] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input3
    [ 1.824737] using rtc device, omap_rtc, for alarms
    [ 1.829620] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
    [ 1.836517] i2c /dev entries driver
    [ 1.840484] Linux video capture interface: v2.00
    [ 1.845489] usbcore: registered new interface driver uvcvideo
    [ 1.851470] USB Video Class driver (1.1.1)
    [ 1.856597] input: lm75-temp as /devices/virtual/input/input4
    [ 1.863098] lm75 2-0048: hwmon0: sensor 'tmp275'
    [ 1.870513] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [ 1.877075] device-mapper: uevent: version 1.0.3
    [ 1.882110] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-d
    evel@redhat.com
    [ 1.890899] Bluetooth: HCI UART driver ver 2.2
    [ 1.895568] Bluetooth: HCI H4 protocol initialized
    [ 1.900543] Bluetooth: HCILL protocol initialized
    [ 1.905456] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
    [ 1.914489] cpuidle: using governor ladder
    [ 1.918884] cpuidle: using governor menu
    [ 1.926422] usbcore: registered new interface driver usbhid
    [ 1.932281] usbhid: USB HID core driver
    [ 2.041625] logger: created 256K log 'log_main'
    [ 2.046478] logger: created 256K log 'log_events'
    [ 2.051452] logger: created 256K log 'log_radio'
    [ 2.056396] logger: created 256K log 'log_system'
    [ 2.061798] usbcore: registered new interface driver snd-usb-audio
    [ 2.069305] _regulator_get: 2-001b supply IOVDD not found, using dummy regula
    tor
    [ 2.077117] _regulator_get: 2-001b supply DVDD not found, using dummy regulat
    or
    [ 2.084777] _regulator_get: 2-001b supply AVDD not found, using dummy regulat
    or
    [ 2.092468] _regulator_get: 2-001b supply DRVDD not found, using dummy regula
    tor
    [ 2.103485] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
    [ 2.110656] ALSA device list:
    [ 2.113769] #0: AM335X EVM
    [ 2.116790] oprofile: hardware counters not available
    [ 2.122070] oprofile: using timer interrupt.
    [ 2.126708] nf_conntrack version 0.5.0 (3930 buckets, 15720 max)
    [ 2.133422] ip_tables: (C) 2000-2006 Netfilter Core Team
    [ 2.139129] TCP cubic registered
    [ 2.142700] NET: Registered protocol family 10
    [ 2.148040] IPv6 over IPv4 tunneling driver
    [ 2.153106] NET: Registered protocol family 17
    [ 2.157745] can: controller area network core (rev 20090105 abi 8)
    [ 2.164367] NET: Registered protocol family 29
    [ 2.169006] can: raw protocol (rev 20090105)
    [ 2.173461] can: broadcast manager protocol (rev 20090105 t)
    [ 2.179595] Bluetooth: RFCOMM TTY layer initialized
    [ 2.184753] Bluetooth: RFCOMM socket layer initialized
    [ 2.190093] Bluetooth: RFCOMM ver 1.11
    [ 2.194030] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [ 2.199554] Bluetooth: BNEP filters: protocol multicast
    [ 2.205017] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [ 2.211334] Registering the dns_resolver key type
    [ 2.216339] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
    rev 3
    [ 2.224334] ThumbEE CPU extension supported.
    [ 2.228851] mux: Failed to setup hwmod io irq -22
    [ 2.234497] Power Management for AM33XX family
    [ 2.239318] Trying to load am335x-pm-firmware.bin (60 secs timeout)
    [ 2.246002] Copied the M3 firmware to UMEM
    [ 2.250274] omap_hwmod: wkup_m3: wkup_m3: hwmod data error: OMAP4 does not su
    pport st_shift
    [ 2.264038] clock: disabling unused clocks to save power
    [ 2.271148] Detected MACID=0:18:31:8e:fe:a0
    [ 2.277557] input: gpio-keys as /devices/platform/gpio-keys/input/input5
    [ 2.284973] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UT
    C (946684800)
    [ 2.294250] Waiting for root device /dev/mmcblk0p2...
    [ 2.379669] mmc0: new high speed SDHC card at address e624
    [ 2.385925] mmcblk0: mmc0:e624 SU08G 7.40 GiB
    [ 2.393035] mmcblk0: p1 p2 p3 p4
    [ 2.506896] mmc1: card claims to support voltages below the defined range. Th
    ese will be ignored.
    [ 2.528686] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
    [ 2.536590] mmc1: new SDIO card at address 0001
    [ 2.758850] EXT4-fs (mmcblk0p2): warning: maximal mount count reached, runnin
    g e2fsck is recommended
    [ 2.770324] EXT4-fs (mmcblk0p2): recovery complete
    [ 2.776733] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. O
    pts: (null)
    [ 2.785278] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [ 2.791961] Freeing init memory: 236K
    [ 2.812530] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_s
    core_adj instead.
    [ 2.917907] init: cannot open '/initlogo.rle'
    [ 2.946777] Disabling lock debugging due to kernel taint
    [ 2.953033] Compat-wireless backport release: compat-wireless-2011-12-05-1-g8
    4dbe2c
    [ 2.960998] Backport based on wl12xx.git v2.6.39-1328-g0890f48
    [ 2.994689] cfg80211: Calling CRDA to update world regulatory domain
    [ 3.052825] (stk) :line disc installation timed out
    [ 3.092864] init: cannot find '/system/etc/install-recovery.sh', disabling 'f
    lash_recovery'
    [ 3.105560] android_usb: already disabled
    [ 3.113983] adb_bind_config
    [ 3.267272] cfg80211: World regulatory domain updated:
    [ 3.272766] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_g
    ain, max_eirp)
    [ 3.281463] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi,
    2000 mBm)
    [ 3.289733] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi,
    2000 mBm)
    [ 3.298004] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi,
    2000 mBm)
    [ 3.306274] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi,
    2000 mBm)
    [ 3.314514] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi,
    2000 mBm)
    [ 3.760406] adb_open
    root@android:/ # [ 4.708862] init: untracked pid 81 exited
    [ 5.173065] (stk) :line disc installation timed out
    [ 7.292846] (stk) :line disc installation timed out
    [ 9.412872] (stk) :line disc installation timed out
    [ 11.532928] (stk) :line disc installation timed out
    [ 13.652893] (stk) :line disc installation timed out
    [ 14.652893] Bluetooth: st_register failed -22
    [ 14.694396] warning: `zygote' uses 32-bit capabilities (legacy support in use
    )
    [ 18.543426] request_suspend_state: wakeup (3->0) at 18540612694 (2000-01-01 0
    0:00:16.750137796 UTC)
    [ 18.733184] init: no such service 'hciattach'
    [ 19.852874] (stk) :line disc installation timed out
    [ 21.003540]
    [ 21.003540] CPSW phy found : id is : 0x4dd074
    [ 21.010406] PHY 0:01 not found
    [ 21.016387] ADDRCONF(NETDEV_UP): eth0: link is not ready
    [ 21.972839] (stk) :line disc installation timed out
    [ 24.092864] (stk) :line disc installation timed out
    [ 25.531616] acc_open
    [ 25.534027] acc_release
    [ 26.212921] (stk) :line disc installation timed out
    [ 28.333221] (stk) :line disc installation timed out
    [ 30.452972] (stk) :line disc installation timed out
    [ 31.452911] Bluetooth: st_register failed -22
    [ 32.672912] (stk) :line disc installation timed out
    [ 34.795959] (stk) :line disc installation timed out
    [ 36.912963] (stk) :line disc installation timed out
    [ 39.032836] (stk) :line disc installation timed out

  • one more.

    I pluged-out Wifi-BT module card and same. This is bad news.

    Then this module not working. But ı've just purchased.

  • I would suggest you discuss with your vendor for replacement.

  • I have the same issue and bt wilink works for some time and not always throwing up line discipline error 

    Pavan suggested some troubleshooting techniques but not working

    Let me know how did you solve it?

  • I couldn't.

    It's completely related SO-DIMM socket contacts. I sent my item via our local TI distributor. They sad me that "it can took 2 or 3 months to fixed part's returning" and i decided to buy new one. Even today my first AM335X board not here. But TI reported that module's problem is related mass production not customer side. I spend Almost 2000$ :( in total. 

    You can see oxide contacts.

  • Hi,

    I had this same error which is solved by the uim  execution before btwilink called.

    http://elinux.org/PandaBoard/Ubuntu_Tips

    Regards,

    Dibin