When I use DM368 resize raw data to YUV420, from 1920x1080 resize to 1920x1080 with ISIF in mode and resize is free run mode in 30fps.
Then encode to 1080P H.264 and vpbe output is 1080P 30fps.It's working.
When I change resizer input size smaller than 960x540 by changing register IPIPE.SRC_VSZ 、 IPIPE.SRC_HSZ、RSZ.RZA_H_DIF、and RSZ.RZA_V_DIF.
And resizer output is 1080P 30fps,some thing error.
Problem1:It resize output like the below image.The image is YUV data transfer to BMP.
YUV data which saved in DDR is below link.
5557.lumens_8242_1920x1088.zip
Problem 2:It's fail for resizer when resizer input decrease to smaller size . The resizer had no new output YUV data.
DM368 is working, when I change the input size as 1080P, it's working again.
I check the display buffer and resizer output buffer are not the same buffer in register setting.
If Resizer scaling up has any limit for input size?
Can I use small data size scaling up to 1080P 30dps?
Any suggestion?
Thanks and regards.
by Alfred