Hi TI experts,
I am using the OMAP3730 based DevKit8500 from Embest running WinCE 6 to develop a system.
Most features work fine. I can:
- Download WinCE Kernel "NK.bin" and use KITL kernel debugger over USB,
- Download WinCE Kernel "NK.bin" over DM9000 ethernet controller.
However I cannot use KITL over DM9000 ethernet controller.
This is VERY annoying, since I try to develop a USB FN kernekl driver, which I cannot debug when using KITL over USB FN, which lock the USB FN driver.
I have seen some related bug reports from 2009, so I believe I am not the first developper to encounter this issue
Any advice ? comment ? bug fix ? KITL Beta source code ?
Thancks in advance
Franck