I have just received a new TEVM4470G-05-10-00 with processor board 4470 GP ES1.0(D) and main board 2158-004.
It will not display a UI on main LCD (on all android binaries I've tested)
- the uboot splash animation is shown so hw is functional
- if I plug in an HDMI the UI is available by mirroring so android is running correctly
- the touchscreen on tablet is also working.
I've attached the boot log from AJ1.1 (http://omappedia.org/wiki/Android:_Working_with_pre-built_binaries).
Can someone help on this?
Thanks, Iain