Other Parts Discussed in Thread: CCSTUDIO, TMS320C6678
Hi,
I'm just trying to get through the System Analyzer tutorial and I hang at step 3.
I use the project from http://processors.wiki.ti.com/index.php/TMS320C6678L_Build_Configuration for C6678 EVM
Building works fine after I set up the correct path, but during linking I get the following ERROR:
'Building target: StairstepEthernet_6678.out'
'Invoking: C6000 Linker'
"C:/ti/ccsv5/tools/compiler/c6000_7.3.8/bin/cl6x" -mv6600 -g --define=_INCLUDE_NIMU_CODE --define=C66_PLATFORMS --define=_NDK_EXTERN_CONFIG --display_error_number --diag_warning=225 --abi=eabi -z -m"StairstepEthernet_6678.map" --warn_sections -i"C:/ti/ccsv5/tools/compiler/c6000_7.3.8/lib" -i"C:/ti/ccsv5/tools/compiler/c6000_7.3.8/include" --reread_libs --rom_model -o "StairstepEthernet_6678.out" -l"./configPkg/linker.cmd" "./stairstep.obj" "./resourcemgr.obj" "./platform_osal.obj" "./netCtrlCallbackFns.obj" "./evmInit.obj" -l"libc.a"
<Linking>
"./configPkg/linker.cmd", line 301: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 301: error #10265: no valid memory range(NULL)
available for placement of "systemHeap"
"./configPkg/linker.cmd", line 301: error #10099-D: run placement fails for
object "systemHeap", size 0xf4240 (page 0)
"./configPkg/linker.cmd", line 272: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 272: error #10265: no valid memory range(NULL)
available for placement of ".text"
"./configPkg/linker.cmd", line 272: error #10099-D: placement fails for object
".text", size 0x5af80 (page 0)
"./configPkg/linker.cmd", line 289: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 289: error #10265: no valid memory range(NULL)
available for placement of ".far"
"./configPkg/linker.cmd", line 289: error #10099-D: run placement fails for
object ".far", size 0x1e928 (page 0)
"./configPkg/linker.cmd", line 284: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 284: error #10265: no valid memory range(NULL)
available for placement of ".const"
"./configPkg/linker.cmd", line 284: error #10099-D: placement fails for object
".const", size 0xa95e (page 0)
"./configPkg/linker.cmd", line 303: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 303: error #10265: no valid memory range(NULL)
available for placement of "platform_lib"
"./configPkg/linker.cmd", line 303: error #10099-D: run placement fails for
object "platform_lib", size 0x1370 (page 0)
"./configPkg/linker.cmd", line 275: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 275: error #10265: no valid memory range(NULL)
available for placement of "GROUP_1"
"./configPkg/linker.cmd", line 275: error #10099-D: run placement fails for
object "GROUP_1", size 0x29f (page 0)
"./configPkg/linker.cmd", line 285: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 285: error #10099-D: run placement fails for
object ".data", size 0x0 (page 0)
"./configPkg/linker.cmd", line 288: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 288: error #10099-D: run placement fails for
object ".sysmem", size 0x0 (page 0)
"./configPkg/linker.cmd", line 302: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 302: error #10099-D: run placement fails for
object ".code", size 0x0 (page 0)
"./configPkg/linker.cmd", line 304: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 304: error #10099-D: run placement fails for
object ".gBuffer", size 0x0 (page 0)
"./configPkg/linker.cmd", line 305: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 305: error #10099-D: run placement fails for
object ".far:WEBDATA", size 0x0 (page 0)
"./configPkg/linker.cmd", line 308: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 308: error #10099-D: placement fails for object
"xdc.meta", size 0x128 (page 0)
>> Compilation failure
"./configPkg/linker.cmd", line 281: warning #10097: memory range not found: DDR
on page 0
"./configPkg/linker.cmd", line 281: error #10265: no valid memory range(NULL)
available for placement of ".cinit"
"./configPkg/linker.cmd", line 281: error #10099-D: placement fails for object
".cinit", size 0xf19 (page 0)
undefined first referenced
symbol in file
--------- ----------------
Osal_paMtCsEnter C:\ti\pdk_C6678_1_1_1_4\packages\ti\drv\pa\lib\ti.drv.pa.ae66<pa.oe66>
Osal_paMtCsExit C:\ti\pdk_C6678_1_1_1_4\packages\ti\drv\pa\lib\ti.drv.pa.ae66<pa.oe66>
error #10234-D: unresolved symbols remain
ELFLNK/build.c:2545:internal fatal error #10251:
("xdc.meta:
This application has requested the Runtime to terminate it in an unusual way.
Please contact the application's support team for more information.
stairstep_Ethernet_pe66.oe66")
INTERNAL ERROR: C:\ti\ccsv5\tools\compiler\c6000_7.3.8\bin\lnk6x.exe aborted
This is a serious problem. Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.: