Team,
Could you please have a look at the below question:
Question regarding the Ethernet GMII interface:
Trying to connect GMII to the Marvell 88E6182 Ethernet switch via its Reverse GMII port. This interface will only be run in gigabit full-duplex mode. From errata DM8168/AM3894 must have a clock present at TX_CLK for the device to boot from LAN in gigabit mode.
1)Can async EMAC[0]_GMCLK be used output to clock the Switch RX_CLK (egress path) then loop back to the TX_CLK ARM pin? What are the timing relations if any to the TXD[0..7] bus
2)As the switch sources the ingress data bus RXD[0..7] with a GTX_CLK which I connect to RX_CLK, can this clock signal be used to go to the TXCLK pin then be tracked (and length matched) with the TXD[7..0] back to the switch?
Will either of these proposals work for errata issue and will it be bootable from Gigabit LAN with these methods?
Thanks and best regards,
Anthony