Other Parts Discussed in Thread: OMAP3530
HI ,all
NOW I encapsulates a decoder on OMAP3530 platform. AND I receive the data stream from local area network. BUT i find some problem.
After decoded 10 frames ,the decoded data will have a problem.and can not be displayed properly.. I save these data into YUV file,and check it.I find there are some 0 in the file . I determine the decoder input data is correct。。I use the same decoder in the CCS and the decoder worked properly..
CAN some body give me some suggestion??? TELL me the possibility reason!!!
thak you all very much!!