This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C672x EMIF Asynchronous Space Question



Hi,

I'm experimenting with the C6720 on a custom built board and I'm booting in parallel flash mode via an 8-bit parallel flash(SST39LF040).  It boots up fine and some sample programs have worked ok, but when I try to read a word from the flash by saying something like this(not actual code, just an example):

#define TOP_OF_ASYNCHRONOUS    0x90000000

#define TOP_OF_INTERNAL_RAM       0x10000000

LDW    .D1     A0, 0x90000004       //Load the contents of memory location 0x90000004 into A0

//4 junk instructions in between to satisfy functional unit latency for the load instruction

LDW    .D1     A1, 0x10000004     //Load Contents of memory location 0x10000004 into A1

Since I'm booting in parallel flash mode, shouldn't the contents of 0x90000004 and 0x100000004 be the same right after boot up?  I have verified that they are not and I'm not really sure why,  I've programmed A1CR with its proper values, I've also programmed all of the SDRAM registers accordingly.  I can read and write from SDRAM fine, but I can't seem to be able to read from my flash.  I also viewed the EM_CS[2] pin on the oscilloscope, while running an infinite loop which tried reading from flash, and the EM_CS[2] pin NEVER went low, while the EM_CS[0] pin was low all the time.  I never touch the cache registers, I also never touch the CSR(control register) which has the settings for the cache.  Could that have something to do with my problem?  

Any comments/tips/answers would be greatly appreciated

  • Hello,

    Some advice:

    At boot time, the first KB of flash EPROM is copied at start of internal RAM: without writing at 0x10000004, the RAM&flash values must be the same.

    As the C6720 has only a program cache, data reads are unaffected by cache status (CSR,...).

    From the above information, CS2 should toggle. If not, some assumption is false; a bad code in the loop test seems the most probable to me (since you seem having no access to an emulator), leading to a read from a wrong address.

    Let the community help you, please give full brute information, especially the A1CR value and the real instructions sequence used for the endless test loop (not a pseudo-code), for example:

    MVKL 0x0004,A2 ; (0x0004 -> A2)

    MVKLH 0x9000,A2 ; (0x9000 -> 16 MSB of A2)

    loop: B loop

    LDW *A2,A0

    NOP 4

    ; A0 loaded and effective branch here

    By the way, there is no functional unit latency on single-word reads, only a 4-cycle delay; you can write:

    LDW *A2,A0

    LDW *A3,A1

    NOP 3

    ; A0 loaded here

    NOP

    ; A1 loaded here

    Jakez

  • Jakez,

    Thank you so much for your advice and help.  I have found the problem and it had nothing to do with the hardware, as it usually is, the issue was on custom assembler! =(.  The funny thing is that I had to communicate with a PIC18F4550 via I2C to read some of the internal registers, to make sure that everything was ok internally and guess what it wasn't, It turns out that when I was using the MVKL and MVKH instructions, my MVKH instruction was translating 0x9000XXXX into 0x8000XXXX, which explains why I was reading SDRAM all the time.  Nonetheless I'd like to thank you for your input once again

    Julxhino