This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BeagleBoard-xm hangs on booting...

hello 

i have BeagleBoard-Xm Rev C runnung ubuntu 11.01 i have Host PC running Ubuntu 12.04.1 when i serially connect it to Host PC it starts booting but sudden stop and hang and then no process happen ahead. Please help me out. when i use Xp host it start booting but stop and hangs on login. please help me.  

  • Please provide more inputs on this issue, like where exactly does the board stop responding, and post the serial log if you have.

  • Hi Mr. chethu. thanks for reply. when i connect my BB-XM to XP host PC via serial connection on Hyper Terminal. it starts running but hangs when login line arrives. when i connect it to Ubuntu 12.04.1 host PC via serial connection using minicom i got something like this

    Welcome to minicom 2.5

    OPTIONS: I18n

    Compiled on May 2 2011, 00:39:27.

    Port /dev/ttyS0

    Press CTRL-A Z for help on special keys

    U-Boot SPL 201-00004-g5726295 2012 - 12:26:50)Instruments Revision detection un0

    reading mg=1000

    reading mg

    U-Boot 2012.0004-g5712 - 12:30/3730-GP ES1.2P2, L3-1lock 1 Ghz

    OMAP board +ready

    D2 MiB

    MiB

    MMP SD/MMC Warningnv() faing defauonment

    In: serial

    Orial

    Erial

    Beaev C

    No EEPROansion bM on expoard

    Die ID #1fca000201607164

    Net: Nalizatioound.

    Hit any key to stop autoboot: 0

    The user button is curre pressedC found e 0

    846 byment from uEnv.txt

    Importing ent from muImage

    3019160 bytes reading

    309781read

    Boom mmc .ooting kom Legacat 80300

    Imag 3.2.13-x7

    Kernel Image (uncompressed)

    Data Siz19096 By9 MiB

    Ent000

    um ... OK

    ## Loading iisk fromImage at Image Name: initramfMDisk Imompressed)

    D: 3097754 Bytess: 00000000000... OK

    Loading Kage ... OK

    OK

    Sternel ..Uncompressing Linux... done, booting the kerne[ 0.000000] Binux on0

    00000] Iing cgros cpuset.000000]izing cg000000] Linux version 3.2.13-x7 gb) (gc2

    [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d

    [ 00] CPU:VIPT nonaliasing data cache, VIPT aliasing instruction cache

    [ 0.000000] Machine: OMAP3 Beagle Board

    [ 0.000000] Beagle expansionboard: 0.000nd expan

    [ 0. SDRAM for VRAM

    [ 0.000000] led, Data cache writeback

    ges/cpu r8192 d27682 (l2cache iva sgsp 192mhz_clk )

    [ n Zone order, mobility grouping on. Total pagesdvi:1280_disp=dvlk0p2 ro roote

    [ hash taies: 204: 65536 entries:000000] [ 0.0y 'cgrou' optionnt memor0.000l

    [ 0.000000] Me6972k/48ailable, 37316k , 0K hig 0.000tual kert:

    [ ector :ffff1000 : 0xfff96 kB)

    vmall- 0xf800 lowmem : 00 - 0xe0 ( 512 M 0xbfe00c000000000000 - 00 ( (

    [ 0init : 00 - 0xc0 ( 343 kB)

    [ 0.000000] .data :c0848ef0 ( 420 kB)

    [ 0.000 : 0xc08f0 ( 785 kB)

    MinObjePUs=1, N[ 0.000000] H

    [ 0.NR_IRQS:410 nr_irqs:410 410

    [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrups

    [ 0.000000] Total of 96 interrupts on 1 active controller

    [ 000] OMAP clockevent source: GPTIMER12 at 32768 Hz

    [ 0.000000] sched32 bits at 32kHzaps ever 0.00olour du

    [ 0.000000] console

    [ 0.038757] minimum:001] Secinitialized

    [ 93] AppArmor: AppArmor initialized

    [ 0.039367] Mount-cache hash table entries: 512

    [ 0.040374] Initializing cgroup subsys cpuacc0.040435] Initiaory

    [ 40527] Is freeze0.040557] Initializing cgroup subsys blkio

    [ 0.040588] Initializing cgroup subsys perf_event

    [ 0.040710] CPU: Testing write buffer coherency: ok

    [ 0.040985]hread -1, cpu 0, socket -1, mpid 0.041656] Brou1687] SMvtmpfs: i

    [ 0.049255] Nstered p0.049468 GPIO haersion 2.5

    [ 0.052856] omap_mux_init: Add partition: #1: core, flags: 0

    [ 0.054138] OMAP3 Beagle Rev: xM C

    [ 0.057617] Reprogramming SDRC clock to 4 0.057678] dpllled: -22 Found N8] 0

    point: dsupported.ble to get DVI reset GPIO

    [ 0.063903dy exists

    [ ck already exist0.065521] OMAP DMA hardware revision 5.0

    [ 0.073425] bio: create slab <bio-0> at 0

    [ 0.074920] SCSI subsystem initialized

    [ 0.076324] usbcore: registered new interface driver usbfs

    [ 0.076477] usbcore: registered new interface driver hub

    [ 0.076721] usbcore: registered new device driver usb

    [ 0.077728] omap_i2c omap_i2c.1: bus 1 rev1.4.0 at 2600 kHz

    [ 0.080444] twl4030: PIH (irq 7) chaining IRQs 368..375

    [ 0.080596] twl4030: power (irq 373) chaining IRQs 376..383

    [ 0.081237] twl4030: gpio (irq 368) chaining IRQs 384..401

    [ 0.081604] _omap_mux_init_gpio: Could not set gpio192

    [ 0.084503] print_constraints: VUSB1V5: 1500 mV normal standby

    [ 0.084991] print_constraints: VUSB1V8: 1800 mV normal standby

    [ 0.085449] print_constraints: VUSB3V1: 3100 mV normal standby

    [ 0.089294] twl4030_usb twl4030_usb: Initialized TWL4030 USB module

    [ 0.090209] print_constraints: VMMC1: 1850 <--> 3150 mV at 3150 mV normal sty

    [ 0.090759] print_constraints: VDAC: 1800 mV normal standby

    [ 0.091217] print_constraints: VAUX2_4030: 1800 mV normal

    [ 0.091674] print_constraints: VDVI: 1800 mV normal standby

    [ 0.092254] print_constraints: VSIM: 1800 <--> 3000 mV at 1800 mV normal stay

    [ 0.092620] omap_i2c omap_i2c.2: bus 2 rev1.4.0 at 400 kHz

    [ 0.103302] omap_i2c omap_i2c.3: bus 3 rev1.4.0 at 100 kHz

    [ 0.104675] NetLabel: Initializing

    [ 0.104705] NetLabel: domain hash size = 128

    [ 0.104736] NetLabel: protocols = UNLABELED CIPSOv4

    [ 0.104827] NetLabel: unlabeled traffic allowed by default

    [ 0.104888] Switching to clocksource 32k_counter

    [ 0.124053] AppArmor: AppArmor Filesystem Enabled

    [ 0.138214] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)

    [ 0.138885] musb-hdrc musb-hdrc: USB OTG mode controller at fa0ab000 using D2

    [ 0.139343] NET: Registered protocol family 2

    [ 0.139739] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

    [ 0.140869] TCP established hash table entries: 16384 (order: 5, 131072 byte)

    [ 0.141235] TCP bind hash table entries: 16384 (order: 5, 131072 bytes)

    [ 0.141601] TCP: Hash tables configured (established 16384 bind 16384)

    [ 0.141632] TCP reno registered

    [ 0.141662] UDP hash table entries: 256 (order: 1, 8192 bytes)

    [ 0.141723] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

    [ 0.142120] NET: Registered protocol family 1

    [ 0.142669] RPC: Registered named UNIX socket transport module.

    [ 0.142700] RPC: Registered udp transport module.

    [ 0.142761] RPC: Registered tcp transport module..142791] RPC: Registered tc.

    [ 0.143096] Trying to unpack rootfs image as initramfs...

    [ 0.460449] Freeing initrd memory: 3024K

    [ 0.460632] omap_dsp_init: 600000 bytes @ 9ee00000

    [ 0.462615] audit: initializing netlink socket (disabled)

    [ 0.462707] type=2000 audit(0.476:1): initialized

    [ 0.678802] VFS: Disk quotas dquot_6.5.2

    [ 0.679321] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

    [ 0.683929] nfs4filelayout_init: NFSv4 File Layout Driver Registering...

    [ 0.684051] fuse init (API version 7.17)

    [ 0.686096] Btrfs loaded

    [ 0.686157] msgmni has been set to 957

    [ 0.687866] Block layer SCSI generic (bsg) driver version 0.4 loaded (major )

    [ 0.687927] io scheduler noop registered

    [ 0.687957] io scheduler deadline registered

    [ 0.688018] io scheduler cfq registered (default)

    [ 0.689025] OMAP DSS rev 2.0

    [ 0.692230] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

    [ 0.693664] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0

    [ 0.694000] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1

    [ 0.694335] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2

    [ 1.466003] console [ttyO2] enabled

    [ 1.470031] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3

    [ 1.4rd: module loaded

    96582] loop: module load[ 1.5adc twl4030_madcsabled, enabling[ 1.5d driveg

    [ 1.5sbcore: registernterfacecdc_ether

    [ 1.532287] usbcore: registered new interface driver rndis_host

    [ 1.538543] cdc_ncm: 04-Aug-2011

    [ 1.542022] usbcore: registered new interface driver cdc_ncm

    [ 1.548492] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

    [ 3.5hci-omapap.0: OMHost Con

    [ 3.572296] ehci-omap ehci-omap.0: new USB b1

    [ 3.580230] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800

    97229] eB 2.0 started, EHCI 1.00.603393] usb usbSB devic idVendor=1d6b, idProdur

    [ 3.623718] usb usb1: Manufacturer: Linux 3.2629699] : Serialub 1-0:1.0: USBd

    [ 3.639160] hub 1-0:1.0: 3 ports detected

    [ 3.667694] Iing USB rage dri[ 3.6sbcore: ed new i driver usb-storage

    [ 3.679290] USB Mass Storage support registered.

    [ 3.684265] usbcore: registered new interface driver libusual

    [ 3.690490] udc: OMAP UDC driver, version: 4 October 2004 (iso) (dma)

    [ 3.697509] gadget: using random self ethernet address

    [ 3.703063] gadget: using random host ethernet address

    [ 3.709777] usb0: MAC 8a:ad:b8:2e:d2:77

    [ 3.713836] usb0: HOST MAC 7a:88:e7:08:6d:89

    [ 3.718383] gadget: Ethernet Gadget, version: Memorial Day 2008

    [ 3.724731] gadget: g_ether ready

    [ 3.728302] musb-hdrc musb-hdrc: MUSB HDRC host driver

    [ 3.734100] musb-hdrc musb-hdrc: new USB bus registered, assigned bus number2

    [ 3.741821] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

    [ 3.748992] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber1

    [ 3.756591] usb usb2: Product: MUSB HDRC host driver

    [ 3.761810] usb usb2: Manufacturer: Linux 3.2.13-x7 musb-hcd

    [ 3.767761] usb usb2: SerialNumber: musb-hdrc

    73040] h.0: USB d

    [ 3.777038] hub 2-0:1.0: 1 port detected

    82073] m PS/2 mouse devin for all mice

    89184] il4030_pwas /devip/omap_i2c.1/i2c9/twl403ton/input/input0

    [ 3.82c /dev driver

    05541] Lia interface: v0.10

    [ 3.809875] lirc Remote Control driver rd, major 249

    [6680] Driver for 1-wire Dallas network protocol.

    [ 3.822845] Ohdog Timx31: inieout 60 [ 3.8wl4030_wdt twl4030_wdt: Failed e

    [ 3.836303] twl4030_wdt: probe of twl4030_wdt failed with err44055] dl (2011-

    r

    [ernor me8] sdhci: Secure Digitalntroller Interface driver

    [ 3.868408] sdhci: Copyright(c) Pierre Ossman

    11352] unew highSB devic 2 using ehci-om[ 4.091033] oc: probe_hsmmc.1with er6

    [ 4.0profile: hardwarvailable

    [ 4.105285] oprofile: usingnterrupt[ 4.1CP cubic registe[ 4.115173] Ns0

    22772] Nstered p7

    [ 4.127624ering th

    [ 4.entor 41 architevariant

    [ 4.140655] CPU extepporr

    [ 4.154663] sr_init: No PMIC hook to rtreflex

    [ 4.160186] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver inid

    [ 4.168457] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver inid

    [ 4.176696] SmartReflex Class3 initialized

    [ 4.186401] clock: disabling locks to save power

    [ 4.193054] uNew USB ound, idVendor=0424, idProduct=9514

    [ 4.200103] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage setup

    [ 4.207061] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage out/status

    [ 4.214447] usb 1-2: New USB device strings: Mfr=0, Product=0, SerialNumber=0

    [ 4.222198] registered taskstats version 1

    [ 4.226684] omapfb omapfb: no driver for display: lcd

    [ 4.232025] fbcvt: 1280x720@60: CVT Name - .921M9-R

    [ 4.238311] h.0: USB d

    [ 4.242401] hub 1-2:1.0: 5 ports d

    [ 4.257537] Cswitching to colour frame 5

    [ 4.275604] regulator_init_complete: complete constraaving on

    [ 4.283294] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

    [ 4.290924] Fnit memo

    18426] u: startion 173

    23736] m0_irq 71End came in a wrong ep0stage setup

    [ 4.430816] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage out/status

    [ 4.499938] mt does nrt readionly swiuming write-enable.

    [ 4.534912] m high sp card at 1234

    [ 4.558868] mmcblk0: 4 SA04G

    74127] u: new hi USB dever 3 usiomap

    [ 4.603912] p1 p2

    38647] u: New US found, =0424, i=ec00

    48992] usb 1-2.1: New US strings: Mfr=0, Product=0, Seri=0

    [ 4.7usb_g_ep0_irq 713: Setup in a wrtage setup

    [ 4.773895] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage out/status

    91699] m0_irq 71End cameong ep0stage setup

    01770] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage out/status

    31817] m0_irq 71End cameong ep0s[ 5.539672] m0_irq 71End came in a wrtage in

    [ 5.769927] Jvalid jo found

    [ 5.778045] E2): error loadinl

    [ 5.859741] m0_irq 71End cametage setup

    67687] m0_irq 71End cameong ep0sstatus

    18750] gadget: ed confiC Ethern

    at this line it stop and do nothing.

    as i am new to this area i dont have enough knowledge please help me..

    thank you very much in advance

    regards

  • hello

    now i have connected USB OTG cable with BB-XM and 5V power supply then i got this

    U-Boot SPL 2012.04-rc1-00004-g5726295 (Apr 01 2012 - 12:26:50)
    Texas Instruments Revision detection unimplemented
    OMAP SD/MMC: 0
    timed out in wait_for_bb: I2C_STAT=1000
    reading u-boot.img
    reading u-boot.img


    U-Boot 2012.04-rc1-00004-g5726295 (Apr 01 2012 - 12:26:50)

    OMAP3630/3730-GP ES1.2, CPU-OPP2, L3-165MHz, Max CPU Clock 1 Ghz
    OMAP3 Beagle board + LPDDR/NAND
    I2C:   ready
    DRAM:  512 MiB
    NAND:  0 MiB
    MMC:   OMAP SD/MMC: 0
    *** Warning - readenv() failed, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Beagle xM Rev C
    No EEPROM on expansion board
    No EEPROM on expansion board
    Die ID #1fca00029ff80000016071641701f00e
    Net:   Net Initialization Skipped
    No ethernet found.
    Hit any key to stop autoboot:  0
    The user button is currently NOT pressed.
    SD/MMC found on device 0
    reading uEnv.txt

    846 bytes read
    Loaded environment from uEnv.txt
    Importing environment from mmc ...
    reading uImage

    3019160 bytes read
    reading uInitrd

    3097818 bytes read
    Booting from mmc ...
    ## Booting kernel from Legacy Image at 80300000 ...
       Image Name:   3.2.13-x7
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    3019096 Bytes = 2.9 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
    ## Loading init Ramdisk from Legacy Image at 81600000 ...
       Image Name:   initramfs
       Image Type:   ARM Linux RAMDisk Image (uncompressed)
       Data Size:    3097754 Bytes = 3 MiB
       Load Address: 00000000
       Entry Point:  00000000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    [    0.000000] Booting Linux on physical CPU 0
    [    0.000000] Initializing cgroup subsys cpuset
    [    0.000000] Initializing cgroup subsys cpu
    [    0.000000] Linux version 3.2.13-x7 (root@panda-a1-1gb) (gcc version 4.6.1 (Ubuntu/Linaro 4.6.1-9ubuntu3) ) #1 SMP Tue Mar 27 12:03:52 UTC 2
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine: OMAP3 Beagle Board
    [    0.000000] Beagle expansionboard: none
    [    0.000000] Beagle second expansionboard: none
    [    0.000000] Reserving 12582912 bytes SDRAM for VRAM
    [    0.000000] Memory policy: ECC disabled, Data cache writeback
    [    0.000000] OMAP3630 ES1.2 (l2cache iva sgx neon isp 192mhz_clk )
    [    0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/600 MHz
    [    0.000000] PERCPU: Embedded 8 pages/cpu @c0d11000 s10784 r8192 d13792 u32768
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125440
    [    0.000000] Kernel command line: console=ttyO2,115200n8 console=tty0 vram=12MB omapfb.mode=dvi:1280x720MR-16@60 omapdss.def_disp=dvi root=/e
    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] allocated 2097152 bytes of page_cgroup
    [    0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups
    [    0.000000] Memory: 494MB = 494MB total
    [    0.000000] Memory: 486972k/486972k available, 37316k reserved, 0K highmem
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    [    0.000000]     vmalloc : 0xe0800000 - 0xf8000000   ( 376 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc07881f0   (7681 kB)
    [    0.000000]       .init : 0xc0789000 - 0xc07dea20   ( 343 kB)
    [    0.000000]       .data : 0xc07e0000 - 0xc0848ef0   ( 420 kB)
    [    0.000000]        .bss : 0xc0848f14 - 0xc090cff0   ( 785 kB)
    [    0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] Hierarchical RCU implementation.
    [    0.000000] NR_IRQS:410 nr_irqs:410 410
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
    [    0.000000] Total of 96 interrupts on 1 active controller
    [    0.000000] OMAP clockevent source: GPTIMER12 at 32768 Hz
    [    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
    [    0.000000] Console: colour dummy device 80x30
    [    0.000000] console [tty0] enabled
    [    0.000671] Calibrating delay loop... 493.67 BogoMIPS (lpj=1929216)
    [    0.038818] pid_max: default: 32768 minimum: 301
    [    0.039093] Security Framework initialized
    [    0.039184] AppArmor: AppArmor initialized
    [    0.039459] Mount-cache hash table entries: 512
    [    0.040435] Initializing cgroup subsys cpuacct
    [    0.040527] Initializing cgroup subsys memory
    [    0.040588] Initializing cgroup subsys devices
    [    0.040618] Initializing cgroup subsys freezer
    [    0.040649] Initializing cgroup subsys blkio
    [    0.040679] Initializing cgroup subsys perf_event
    [    0.040802] CPU: Testing write buffer coherency: ok
    [    0.041076] CPU0: thread -1, cpu 0, socket -1, mpidr 0
    [    0.041748] Brought up 1 CPUs
    [    0.041778] SMP: Total of 1 processors activated (493.67 BogoMIPS).
    [    0.042846] devtmpfs: initialized
    [    0.048980] print_constraints: dummy:
    [    0.049346] NET: Registered protocol family 16
    [    0.049560] GPMC revision 5.0
    [    0.051147] OMAP GPIO hardware version 2.5
    [    0.052978] omap_mux_init: Add partition: #1: core, flags: 0
    [    0.054229] OMAP3 Beagle Rev: xM C
    [    0.057800] Reprogramming SDRC clock to 400000000 Hz
    [    0.057830] dpll3_m2_clk rate change failed: -22
    [    0.059631] Found NAND on CS0
    [    0.059661] Registering NAND on CS0
    [    0.059997] Unable to get DVI reset GPIO
    [    0.060150] hw-breakpoint: debug architecture 0x4 unsupported.
    [    0.060791] Could not look up mcpdm hw_mod
    [    0.064086]  omap-mcbsp.2: alias fck already exists
    [    0.064270]  omap-mcbsp.3: alias fck already exists
    [    0.065673] OMAP DMA hardware revision 5.0
    [    0.073577] bio: create slab <bio-0> at 0
    [    0.075073] SCSI subsystem initialized
    [    0.076446] usbcore: registered new interface driver usbfs
    [    0.076629] usbcore: registered new interface driver hub
    [    0.076843] usbcore: registered new device driver usb
    [    0.077850] omap_i2c omap_i2c.1: bus 1 rev1.4.0 at 2600 kHz
    [    0.080627] twl4030: PIH (irq 7) chaining IRQs 368..375
    [    0.080780] twl4030: power (irq 373) chaining IRQs 376..383
    [    0.081390] twl4030: gpio (irq 368) chaining IRQs 384..401
    [    0.081787] _omap_mux_init_gpio: Could not set gpio192
    [    0.084686] print_constraints: VUSB1V5: 1500 mV normal standby
    [    0.085174] print_constraints: VUSB1V8: 1800 mV normal standby
    [    0.085632] print_constraints: VUSB3V1: 3100 mV normal standby
    [    0.089508] twl4030_usb twl4030_usb: Initialized TWL4030 USB module
    [    0.090393] print_constraints: VMMC1: 1850 <--> 3150 mV at 3150 mV normal standby
    [    0.090942] print_constraints: VDAC: 1800 mV normal standby
    [    0.091400] print_constraints: VAUX2_4030: 1800 mV normal
    [    0.091857] print_constraints: VDVI: 1800 mV normal standby
    [    0.092437] print_constraints: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby
    [    0.092803] omap_i2c omap_i2c.2: bus 2 rev1.4.0 at 400 kHz
    [    0.103515] omap_i2c omap_i2c.3: bus 3 rev1.4.0 at 100 kHz
    [    0.104888] NetLabel: Initializing
    [    0.104919] NetLabel:  domain hash size = 128
    [    0.104949] NetLabel:  protocols = UNLABELED CIPSOv4
    [    0.105010] NetLabel:  unlabeled traffic allowed by default
    [    0.105072] Switching to clocksource 32k_counter
    [    0.124267] AppArmor: AppArmor Filesystem Enabled
    [    0.138427] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
    [    0.139099] musb-hdrc musb-hdrc: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
    [    0.139526] NET: Registered protocol family 2
    [    0.139953] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.141052] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
    [    0.141448] TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
    [    0.141815] TCP: Hash tables configured (established 16384 bind 16384)
    [    0.141845] TCP reno registered
    [    0.141876] UDP hash table entries: 256 (order: 1, 8192 bytes)
    [    0.141906] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    [    0.142333] NET: Registered protocol family 1
    [    0.142852] RPC: Registered named UNIX socket transport module.
    [    0.142913] RPC: Registered udp transport module.
    [    0.142913] RPC: Registered tcp transport module.
    [    0.142974] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.143280] Trying to unpack rootfs image as initramfs...
    [    0.460723] Freeing initrd memory: 3024K
    [    0.460906] omap_dsp_init: 600000 bytes @ 9ee00000
    [    0.462890] audit: initializing netlink socket (disabled)
    [    0.462982] type=2000 audit(0.476:1): initialized
    [    0.679077] VFS: Disk quotas dquot_6.5.2
    [    0.679626] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [    0.684204] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.684326] fuse init (API version 7.17)
    [    0.686370] Btrfs loaded
    [    0.686431] msgmni has been set to 957
    [    0.688171] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
    [    0.688201] io scheduler noop registered
    [    0.688232] io scheduler deadline registered
    [    0.688293] io scheduler cfq registered (default)
    [    0.689300] OMAP DSS rev 2.0
    [    0.692474] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [    0.693908] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
    [    0.694274] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
    [    0.694610] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
    [    1.466339] console [ttyO2] enabled
    [    1.470367] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3
    [    1.488800] brd: module loaded
    [    1.496948] loop: module loaded
    [    1.501586] twl4030_madc twl4030_madc: clk disabled, enabling
    [    1.509582] omap2-nand driver initializing
    [    1.514282] No NAND device found
    [    1.517883] No NAND device found
    [    1.521545] OneNAND driver initializing
    [    1.526367] usbcore: registered new interface driver cdc_ether
    [    1.532623] usbcore: registered new interface driver rndis_host
    [    1.538879] cdc_ncm: 04-Aug-2011
    [    1.542358] usbcore: registered new interface driver cdc_ncm
    [    1.548797] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    3.566162] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
    [    3.572509] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
    [    3.580444] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
    [    3.597473] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
    [    3.603607] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [    3.610778] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    3.618377] usb usb1: Product: OMAP-EHCI Host Controller
    [    3.623962] usb usb1: Manufacturer: Linux 3.2.13-x7 ehci_hcd
    [    3.629913] usb usb1: SerialNumber: ehci-omap.0
    [    3.635406] hub 1-0:1.0: USB hub found
    [    3.639404] hub 1-0:1.0: 3 ports detected
    [    3.667907] Initializing USB Mass Storage driver...
    [    3.673187] usbcore: registered new interface driver usb-storage
    [    3.679534] USB Mass Storage support registered.
    [    3.684509] usbcore: registered new interface driver libusual
    [    3.690734] udc: OMAP UDC driver, version: 4 October 2004 (iso) (dma)
    [    3.697753]  gadget: using random self ethernet address
    [    3.703308]  gadget: using random host ethernet address
    [    3.710052] usb0: MAC b2:6e:58:9c:db:c3
    [    3.714080] usb0: HOST MAC 1a:9b:0a:eb:b7:c2
    [    3.718658]  gadget: Ethernet Gadget, version: Memorial Day 2008
    [    3.725006]  gadget: g_ether ready
    [    3.728576] musb-hdrc musb-hdrc: MUSB HDRC host driver
    [    3.734344] musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 2
    [    3.742095] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    [    3.749237] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    3.756866] usb usb2: Product: MUSB HDRC host driver
    [    3.762084] usb usb2: Manufacturer: Linux 3.2.13-x7 musb-hcd
    [    3.768005] usb usb2: SerialNumber: musb-hdrc
    [    3.773284] hub 2-0:1.0: USB hub found
    [    3.777313] hub 2-0:1.0: 1 port detected
    [    3.782318] mousedev: PS/2 mouse device common for all mice
    [    3.789428] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input0
    [    3.801452] i2c /dev entries driver
    [    3.805786] Linux media interface: v0.10
    [    3.810150] lirc_dev: IR Remote Control driver registered, major 249
    [    3.816925] Driver for 1-wire Dallas network protocol.
    [    3.823120] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
    [    3.829925] twl4030_wdt twl4030_wdt: Failed to register misc device
    [    3.836547] twl4030_wdt: probe of twl4030_wdt failed with error -16
    [    3.844299] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
    [    3.853729] cpuidle: using governor ladder
    [    3.858032] cpuidle: using governor menu
    [    3.862182] sdhci: Secure Digital Host Controller Interface driver
    [    3.868682] sdhci: Copyright(c) Pierre Ossman
    [    4.011566] usb 1-2: new high-speed USB device number 2 using ehci-omap
    [    4.091247] omap_hsmmc: probe of omap_hsmmc.1 failed with error -16
    [    4.100128] oprofile: hardware counters not available
    [    4.105438] oprofile: using timer interrupt.
    [    4.111053] TCP cubic registered
    [    4.115356] NET: Registered protocol family 10
    [    4.122924] NET: Registered protocol family 17
    [    4.127777] Registering the dns_resolver key type
    [    4.132781] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [    4.140838] ThumbEE CPU extension supported.
    [    4.145355] Registering SWP/SWPB emulation handler
    [    4.154846] sr_init: No PMIC hook to init smartreflex
    [    4.160369] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
    [    4.168640] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
    [    4.176879] SmartReflex Class3 initialized
    [    4.186584] clock: disabling unused clocks to save power
    [    4.193267] usb 1-2: New USB device found, idVendor=0424, idProduct=9514
    [    4.200286] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage setup
    [    4.207275] usb 1-2: New USB device strings: Mfr=0, Product=0, SerialNumber=0
    [    4.214996] registered taskstats version 1
    [    4.219482] omapfb omapfb: no driver for display: lcd
    [    4.224822] fbcvt: 1280x720@60: CVT Name - .921M9-R
    [    4.231170] hub 1-2:1.0: USB hub found
    [    4.235229] hub 1-2:1.0: 5 ports detected
    [    4.250366] Console: switching to colour frame buffer device 160x45
    [    4.268432] regulator_init_complete: VDAC: incomplete constraints, leaving on
    [    4.276123] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
    [    4.283752] Freeing init memory: 340K
    [    4.411132] udevd[61]: starting version 173
    [    4.423126] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage setup
    [    4.430297] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage out/status
    [    4.500488] mmc0: host does not support reading read-only switch. assuming write-enable.
    [    4.537475] mmc0: new high speed SDHC card at address 1234
    [    4.566619] usb 1-2.1: new high-speed USB device number 3 using ehci-omap
    [    4.581909] mmcblk0: mmc0:1234 SA04G 3.67 GiB
    [    4.612213]  mmcblk0: p1 p2
    [    4.746856] usb 1-2.1: New USB device found, idVendor=0424, idProduct=ec00
    [    4.757293] usb 1-2.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
    [    4.768066] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage setup
    [    4.991088] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage setup
    [    5.001281] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage out/status
    [    5.331085] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage setup
    [    5.539093] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage in/status
    [    5.640533] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
    [    5.651580] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
    [    5.686767] JBD2: no valid journal superblock found
    [    5.695220] EXT4-fs (mmcblk0p2): error loading journal
    [    5.859100] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage setup
    [    6.067077] musb_g_ep0_irq 713: SetupEnd came in a wrong ep0stage in/status
    [    6.720123]  gadget: full-speed config #1: CDC Ethernet (EEM)
     

    now on this line it stops and show me nothing ahead. please bro tell me where i am going wrong.

    thanks

    regards.

  • Please somebody tell me how to repair this??

  • Hi,

    mount the sd card on your computer and check the file system. I guess the filesystem is corrupted due to abrupt poweroff.

    do sudo fsck /dev/sdb2 (assuming your sd card is /dev/sdb)

    and update the result.

    In case of any error related to superblocks,  try formatting your /dev/sdb2 and copy the file system image freshly.