This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UPP Recieve Problem

Expert 2370 points

Other Parts Discussed in Thread: OMAP-L138

Hi,

I modified evmomapl138_test_upp example to use UPP's channel A to recieve data from ADC attached to the UI board of the OMAP-L138 EVM. I don't get a proper 100 kHz sine wave after configuring CHN bit in UPTCL register to zero but it does work with CHN = 1 (dual channel mode). Why is that ?

Moreover, I enabled EOWI interrupt but it doesn't trigger to enter the ISR. I followed Sample Interrupt Service Routine given in section 2.6.4 of uPP User Guide to write ISR but I am not sure if that's written correctly. I also don't understand how could I enable next DMA transfer so that DMA continues to capture sampled data from ADC ?

Following are the code snippet:

int32_t executeTest(void)
{    
    upp_config_t config;
    UPXS2_t    * UPIS2r = (UPXS2_t *)&(UPP->UPIS2);
    

    //UPCTL
    config.UPCTL.value=0;
    config.UPCTL.bits.DPFA = 0;
    config.UPCTL.bits.DPWA = 2;       //10 bit data
    config.UPCTL.bits.IWA = 1;          //16 bit interface
    config.UPCTL.bits.CHN = 1;          //dual channel mode
    config.UPCTL.bits.MODE = 0;       //0 all recv, 1 all xmit, 2 a recv b xmit, 3 a xmit b recv

    //UPICR
    config.UPICR.value=0;

    //UPIVR
    config.UPIVR.value=0;
    config.UPIVR.bits.VALA = 0x0000;

    //UPTCR
    config.UPTCR.value=0;                //all values 0 for 64byte DMA bursts read / write
    //config.UPTCR.bits.RDSIZEI =  3;

    //UPDLB
    config.UPDLB.value=0;                //no loopback      

    //UPIES                            
    config.UPIES.bits.EOWI= 1;            //turn on EOW(end of window) interrupt
  

    //UPPCR
    config.UPPCR.value = 0;                
    config.UPPCR.bits.EN = 1;               //enable uPP
    config.UPPCR.bits.RTEMU = 1;        //allow emulator use
    config.UPPCR.bits.SOFT = 1;           //allow emulation

    UPP_init(&config);

    UPP->UPID0 = (uint32_t)&recv_buffer;         //add next DMA transfer
    UPP->UPID1 = 0x00010800;                      //1 lines 128 bytes per line
    UPP->UPID2 = 0x00000800;                     //no offset between lines
    while(UPIS2r->bits.PEND == 1){};
}

interrupt void upp_isr(void)
{
 
  UPISR_t interrupt_status;
  interrupt_status.value = UPP->UPIER;
 
  while (interrupt_status.value != 0)
  {
    
    if (interrupt_status.bits.EOWI)
    {
        interrupt_status.bits.EOWI = 1;     // clear EOWI
         // Handle EOWI
    }

    // loop again if any interrupts are left
    interrupt_status.value = UPP->UPIER;
  } // end of while
 
  // write end of interrupt vector to allow future calls
  UPP->UPEOI = 0;
 
} // end of function

I would really appreciate your quick help.

Regards,

BAS