This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP/BIOS configuraion file for EVM6657



Hi,

I am using CCS5.2.1 and I have installed bios_mcsdk_2_1_1.

I want to create a DSP/BIOS configuraion file for EVM6657 (File->New->DSP/BIOS v5.x configuration).  But I didn't find evm6657 (xdctools_3_23_04_60/packages/ti/platforms) in platform selection menu.

Do I need to install any other package to get the platform listing in the menu?

  • Bhanu,

    There is no support for *DSP/BIOS* on the C66 devices.  You’ll need to use *SYS/BIOS*.  

    It would be easiest if you start with a pre-existing example application template, run that app, and then modify it as appropriate for your application.

    Scott