This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure ISP capture raw data from parallel input and then output to memory ?



Hi,

I have some problems when writing  a  RAW data camera driver on  AM/DM37x.   Hope your kindly helps !

I want to capture raw data from parallel input of CCDC and output directly to the memory ,but I don't know what is the nessssary step to configure the CCDC and CSIPHY.

Followings are my configuration.

1.    The cam_mclk have been set and workwell.I can get
      HS_VS interrupt from CCDC.but I couldn't get any data from memory that set by CCDC_SDR_ADDR .

2.    CONTROL_CAMERA_PHY_CTRL[1:0] = 11 (GPI mode)

       CONTROL_CAMERA_PHY_CTRL[2:3] = 11  (GPI mode)

       CCDC_SYN_MODE[18] VP2SDR = 0x1

       CCDC_SYN_MODE[17] WEN = 0x1

       CCDC_SYN_MODE[16] VDHDEN = 0x1

       CCDC_SYN_MODE [13:12] INPMOD = 0

      CCDC_SYN_MODE [10:8] DATSIZ = 0x6

     (CCDC_SYN_MODE[31:0] = 0x70604)


      CCDC_REC656IF[0] R656ON = 0x0

     CCDC_SDR_ADDR [31:0] ADDR = 0x86094000 ( allocated physical memory address )

     ISP_CTRL[31:0 ] = 0x9C100

 

3,  I didn't get any data in the allcated momery( 0x86094000 )  when HS_VS interrupt occur.

So,Could do you please tell me  how to let the CCDC read the data from parallel input and write the data to memory ?

Should I set the "CSI1/CCP2B or CSI2 Receiver Associated PHY" and how to setup it ?

 

Thanks

Fan