Hi,
In DSP Link version 1_65_01_06, it provides a sample code named LOOP. When i tried to execute this application, i got error as PROC_start failed. Status = [0x80008052]. Does anyone have an idea why this fails. The error print in as shown below
DSP-side configuration mismatch/failure
0 -> success
Positive value -> DSP-side failure code.
(Uint32) -1 -> DSP-side component was not initialized.
DRV configuration status [0xffffffff]
IPS configuration status [0xffffffff]
POOL configuration status [0xffffffff]
MPCS configuration status [0xffffffff]
MPLIST configuration status [0xffffffff]
MQT configuration status [0xffffffff]
DATA configuration status [0xffffffff]
RingIO configuration status [0xffffffff]
PROC_start failed. Status = [0x80008052]