Other Parts Discussed in Thread: TLC59108, TVP7002
Hi,
I have some problem running Capture Encode Demo on TI8148_EVM.
root@dm814x-evm:~# lsmod
Module Size Used by
bufferclass_ti 4950 0
omaplfb 10746 0
pvrsrvkm 155434 2 bufferclass_ti,omaplfb
tlc59108 1545 0
ti81xxhdmi 17685 0
ti81xxvin 20591 0
tvp7002 6429 1
ti81xxvo 21210 0
ti81xxfb 21979 2
vpss 74936 5 omaplfb,ti81xxhdmi,ti81xxvin,ti81xxvo,ti81xxfb
syslink 1125041 0
ipv6 209855 14
I can boot without problem the board and all modules and drivers seem to be loaded, but when I try to run "1080p30 Capture and Encode" on Matrix Applications the LCD goes black and I have to kill the process.
root@dm814x-evm:~# VPSS_GRPX : please open fb1 node first.
root@dm814x-evm:~#
root@dm814x-evm:~# ps
PID USER VSZ STAT COMMAND
1 root 1708 S init [5]
2 root 0 SW [kthreadd]
3 root 0 SW [ksoftirqd/0]
4 root 0 SW [kworker/0:0]
5 root 0 SW [kworker/u:0]
6 root 0 SW< [khelper]
7 root 0 SW [irq/72-serial i]
8 root 0 SW [irq/73-serial i]
9 root 0 SW [irq/74-serial i]
10 root 0 SW [irq/44-serial i]
11 root 0 SW [irq/45-serial i]
12 root 0 SW [irq/46-serial i]
13 root 0 SW< [mboxd]
14 root 0 SW [sync_supers]
15 root 0 SW [bdi-default]
16 root 0 SW< [kblockd]
17 root 0 SW< [omap2_mcspi]
18 root 0 SW [khubd]
19 root 0 SW [kseriod]
20 root 0 SW< [kmmcd]
21 root 0 SW< [musb-hdrc.0]
22 root 0 SW< [musb-hdrc.1]
23 root 0 SW< [rpciod]
24 root 0 SW [kswapd0]
25 root 0 SW [kworker/0:1]
26 root 0 SW< [aio]
27 root 0 SW< [nfsiod]
28 root 0 SW< [crypto]
35 root 0 SW [scsi_eh_0]
36 root 0 SW [kworker/u:1]
37 root 0 SW [kworker/u:2]
38 root 0 SW [mtdblock0]
39 root 0 SW [mtdblock1]
40 root 0 SW [mtdblock2]
41 root 0 SW [mtdblock3]
42 root 0 SW [mtdblock4]
43 root 0 SW [mtdblock5]
48 root 0 SW [irq/191-qt60224]
49 root 0 SW< [usbhid_resumer]
69 root 2276 S < /sbin/udevd -d
1224 root 0 SW< [HDMI WQ]
1240 messageb 3324 S /usr/bin/dbus-daemon --system
1251 root 2240 S /usr/sbin/dropbear -r /etc/dropbear/dropbear_rsa_host
1256 root 2936 S /usr/sbin/telnetd
1261 root 2524 S /usr/sbin/netserver
1266 root 3000 S /sbin/syslogd -n -C64 -m 20
1268 root 2936 S /sbin/klogd -n
1273 root 2172 S /usr/sbin/thttpd -d /srv/www -p 8080 -u root -c /cgi-
1298 root 0 SW< [pvr_timer]
1330 root 0 SW< [pvr_workqueue]
1344 root 114m S /usr/bin/matrix_guiE -qws /usr/share/matrix/html/menu
1351 root 2516 S login -- root
1352 root 1968 S /sbin/getty 38400 tty1
1357 root 3128 S -sh
1360 root 2940 S /bin/sh /usr/bin/runCaptureEncode
1367 root 242m S ./capture_encode_a8host_debug.xv5T -o sample.h264 -m
1378 root 3128 R ps
root@dm814x-evm:~# kill 1367
root@dm814x-evm:~# notify_shm_drv_sendevent failed! status = 0xfffffff2
notify_send_event failed! status = 0xfffffff2
VPSS_GRPX : please open fb1 node first.
Then I try to stop the matrix-gui and pvr-init and run the demo from the console, but in this case the system hangs and I have to reset the board.
Here the log of the boot with the environment and the capture_encode_a8host_debug.xv5T error:
U-Boot 2010.06 (Apr 30 2012 - 01:02:37)
TI8148-GP rev 2.1
ARM clk: 600MHz
DDR clk: 400MHz
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
Using default environment
The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is alr
eady flashed
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x20000, size 0x40000
262144 bytes read: OK
## Starting application at 0x81000000 ...
U-Boot 2010.06 (Apr 30 2012 - 00:57:34)
TI8148-GP rev 2.1
ARM clk: 600MHz
DDR clk: 400MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
MMC: OMAP SD/MMC: 0
.:;rrr;;.
,5#@@@@#####@@@@@@#2,
,A@@@hi;;;r5;;;;r;rrSG@@@A,
r@@#i;:;s222hG;rrsrrrrrr;ri#@@r
:@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:
B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B
@@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@
@@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@
@@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@
G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G
@9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@
X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
@#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
@A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
@&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
@#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
:@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
@@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@
@A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@
;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;
r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r
,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,
B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H
.@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.
.A@@#5r;;;r;;;rrr;r:r#AsM@@H.
;&@@@@MhXS5i5SX9B@@@@G;
:ihM#@@@@@##hs,
Net: Detected MACID:40:5f:c2:40:f6:e1
cpsw
Hit any key to stop autoboot: 0
TI8148_EVM#printenv
verify=yes
ramdisk_file=ramdisk.gz
loadaddr=0x81000000
script_addr=0x80900000
loadbootscript=fatload mmc 0 ${script_addr} boot.scr
bootscript= echo Running bootscript from MMC/SD to set the ENV...; source ${scri
pt_addr}
ethaddr=40:5f:c2:40:f6:e1
ethact=cpsw
logotime=15
filesize=2507A
fileaddr=81000000
gatewayip=192.168.100.1
netmask=255.255.254.0
ipaddr=192.168.100.111
dnsip=192.168.100.1
bootdelay=4
baudrate=115200
oldbootargs=console=ttyO0,115200n8 rootwait rw mem=364M@0x80000000 mem=320M@0x9F
C00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 root=/dev/nfs nfsroot=192.168.
100.229:/home/user/targetfs ip=dhcp
autoload=no
oldserverip=192.168.100.229
serverip=192.168.100.67
oldbootfile=uImage
bootfile=uImage
oldbootcmd=dhcp;setenv serverip 192.168.100.229;tftpboot;bootm
bootcmd=dhcp;setenv serverip 192.168.100.67;tftpboot;bootm
bottargs=
bootargs=console=ttyO0,115200n8 rootwait rw mem=364M@0x80000000 mem=320M@0x9FC00
000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 vram=50M ti816xfb.vram=0:16M,1:16
M,2:6M root=/dev/nfs nfsroot=192.168.100.67:/home/user/targetfs ip=dhcp
Environment size: 1102/8188 bytes
TI8148_EVM#boot
link up on port 0, speed 1000, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.100.66
link up on port 0, speed 1000, full duplex
Using cpsw device
TFTP from server 192.168.100.67; our IP address is 192.168.100.66
Filename 'uImage'.
Load address: 0x81000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
############
done
Bytes transferred = 2720256 (298200 hex)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2720192 Bytes = 2.6 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (user@Ubuntu) (gcc version 4.3.3 (Sourcery G++ Lite
2009q1-203) ) #1 Fri Oct 19 13:24:13 CEST 2012
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148evm
vram size = 52428800 at 0x0
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 2.1
SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 160648
Kernel command line: console=ttyO0,115200n8 rootwait rw mem=364M@0x80000000 mem=
320M@0x9FC00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 vram=50M ti816xfb.vra
m=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=192.168.100.67:/home/user/targetfs ip=
dhcp
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 364MB 270MB = 634MB total
Memory: 637476k/637476k available, 62940k reserved, 276480K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd7000000 - 0xf8000000 ( 528 MB)
lowmem : 0xc0000000 - 0xd6c00000 ( 364 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003c000 ( 208 kB)
.text : 0xc003c000 - 0xc0525000 (5028 kB)
.data : 0xc0526000 - 0xc0571780 ( 302 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 598.01 BogoMIPS (lpj=2990080)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
NOR: Can't request GPMC CS
Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd7020000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea2080b
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
pcf857x 1-0021: gpios 128..143 on a pcf8575
regulator: VRTC: 1800 mV
regulator: VIO: 1500 mV
regulator: VDD1: 600 <--> 1500 mV at 1200 mV
regulator: VDD2: 600 <--> 1500 mV at 1200 mV
regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV
regulator: LDO1: 1100 <--> 3300 mV at 1800 mV
regulator: LDO2: 1100 <--> 3300 mV at 1800 mV
regulator: LDO3: 1100 <--> 3300 mV at 3300 mV
regulator: LDO4: 1100 <--> 3300 mV at 1800 mV
regulator: LDO5: 1100 <--> 3300 mV at 3300 mV
regulator: LDO6: 1100 <--> 3300 mV at 3300 mV
regulator: LDO7: 1100 <--> 3300 mV at 3300 mV
regulator: LDO8: 1100 <--> 3300 mV at 1800 mV
tps65910 1-002d: No interrupt support, no core IRQ
omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d701e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d7026800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
highmem bounce pool size: 64 pages
JFFS2 version 2.2. (NAND) �ũ 2001-2006 Red Hat, Inc.
msgmni has been set to 705
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x1
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
usb 2-1: new low speed USB device using musb-hdrc and address 2
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffc
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
d_can d_can: d_can device registered (irq=52, irq_obj=53)
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapter
s
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
usb 2-1: New USB device found, idVendor=04f3, idProduct=0234
usb 2-1: New USB device strings: Mfr=0, Product=2, SerialNumber=0
usb 2-1: Product: OM
ata1: SATA link down (SStatus 0 SControl 300)
qt602240_ts 1-004a: Family ID: 128 Variant ID: 1 Version: 22 Build: 171
qt602240_ts 1-004a: Matrix X Size: 18 Matrix Y Size: 12 Object Num: 17
input: AT42QT602240/ATMXT224 Touchscreen as /devices/platform/omap/omap_i2c.1/i2
c-1/1-004a/input/input0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
input: OM as /devices/platform/omap/ti81xx-usbss/musb-hdrc.1/usb2/2-1/2-1:1.0/in
put/input1
generic-usb 0003:04F3:0234.0001: input: USB HID v1.11 Mouse [OM] on usb-musb-hdr
c.1-1/input0
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated for remote proc id 2 at physical Address 0x
bf900000
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=40:5f:c2:40:f6:e1
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
CPSW phy found : id is : 0x4dd074
CPSW phy found : id is : 0x4dd074
Sending DHCP requests .
PHY: 0:00 - Link is Up - 1000/Full
PHY: 0:01 - Link is Up - 0/Half
PHY: 0:01 - Link is Down
., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.100.66
IP-Config: Complete:
device=eth0, addr=192.168.100.66, mask=255.255.254.0, gw=192.168.100.1,
host=fw.domain.lan, domain=domain.lan, nis-domain=(none),
bootserver=0.0.0.0, rootserver=192.168.100.67, rootpath=
VFS: Mounted root (nfs filesystem) on device 0:15.
devtmpfs: mounted
Freeing init memory: 208K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udevd (69): /proc/69/oom_adj is deprecated, please use /proc/69/oom_score_adj in
stead.
Root filesystem already rw, not remounting
Caching udev devnodes
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
NOT configuring network interfaces: / is an NFS mount
Thu Oct 11 11:18:00 UTC 2012
INIT: Entering runlevel: 5
Loading HDVICP2 Firmware
DM814X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000001
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00050002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0xeafffffe
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0xeafffffe
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM Initialization completed
SysLink version : 2.20.00.14
SysLink module created on Date:Oct 19 2012 Time:17:43:14
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mma
p <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by
M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
Firmware Loader debugging not configured
Default FL_DEBUG: warning
Allowed FL_DEBUG levels: error, warning, info, debug, log
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: 1 start Successful
Loading HDVPSS (V4L2) Firmware
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mma
p <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by
M3
FIRMWARE: isI2cInitRequiredOnM3: 0
FIRMWARE: Default memory configuration is used
Firmware Loader debugging not configured
Default FL_DEBUG: warning
Allowed FL_DEBUG levels: error, warning, info, debug, log
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: 2 start Successful
Configuring fb0 to LCD
tvp7002 3-005d: tvp7002 found @ 0x5d (OMAP I2C adapter)
tvp7002 3-005d: Rev. 02 detected.
ti81xxvin ti81xxvin: registered sub device tvp7002
ti81xxvin ti81xxvin: TI81xx HDVPSS Capture driver initialized
HDMI W1 rev 4.0
HDMI CEC Spec version 1.2
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
/dev/mem opened.
Memory mapped at address 0x40276000.
Read at address 0x48180F04 (0x40276f04): 0x00000001
Write at address 0x48180F04 (0x40276f04): 0x00000000, readback 0x00000000
/dev/mem opened.
Memory mapped at address 0x40045000.
Read at address 0x48180900 (0x40045900): 0x00000102
Write at address 0x48180900 (0x40045900): 0x00000002, readback 0x00000002
/dev/mem opened.
Memory mapped at address 0x4011a000.
Read at address 0x48180920 (0x4011a920): 0x00040002
Write at address 0x48180920 (0x4011a920): 0x00000002, readback 0x00000002
Starting Matrix GUI application.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm814x-evm ttyO0
Arago 2011.09 dm814x-evm ttyO0
dm814x-evm login: root
root@dm814x-evm:~# /etc/init.d/matrix-gui-e stop
Stopping Matrix GUI application.
root@dm814x-evm:~# /etc/init.d/pvr-init stop
Stopping PVR
root@dm814x-evm:~# /usr/share/ti/ti-omx/capture_encode_a8host_debug.xv5T -o samp
le.h264 -m 1080p -f 60 -b 1000000 -n 1000 -d 0
output file: sample.h264
bit_rate: 1000000
frame_rate: 60
num_frames: 1000
mode: 1080p
display_id: 0
Capture-Encode example
===============================
OMX_Init completed
UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
openeing file
capture compoenent is created
control TVP compoenent is created
Buffer Size computed: 3110400
set input port params (width = 1920, height = 1080)enable capture output port
got eventEnable/Disable Event
dei compoenent is created
set input port params (width = 1920, height = 1080)
set output port params (width = 1920, height = 1080)set output port params (widt
h = 1920, height = 1080)set number of channelsset input resolutionset output res
olutionenable dei input port
got eventEnable/Disable Event
enable dei output port 0
got eventEnable/Disable Event
enable dei output port 1
got eventEnable/Disable Event
encoder compoenent is created
found handle 0x12f4f8 for component OMX.TI.VPSSM3.VFDC
got display handle
found handle 0x133500 for component OMX.TI.VPSSM3.CTRL.DC
Buffer Size computed: 4147200
set input port params (width = 1920, height = 1080)setting input and output memo
ry type to defaultenable input port
got eventEnable/Disable Event
connect call for capture-Dei
connect call for dei- encoder
connect call for dei-display
got event*** unrecoverable error: OMX_ErrorUndefined (0x80001001)
Press a key to proceed
How can I capture video from EVMDM8148?
What are the specifications of the sensor connected to the following inputs?
- "Parallel camera connector"
- VGA input
- DVI input
- composite input
To capture the video through a GStreamer pipeline where do I connect the sensor?
Thanks for any suggestion