Hi,
I'm trying out the aic3204 demo code that came with the C5535 eZdsp example code package, but I'm getting some odd results. Instead of having the headphones and microphone connected to the development board, I have a function generator connected to the line in, and an oscilloscope connected to both line in and line out. The first part of the program, where a 1 kHz signal is being generated, works fine. But when the system is supposed to sample the line in, and replicate the signal on line out, I get the results as shown in the attached figured, where the yellow signal is the signal from the function generator (500 Hz), and the blue signal is the output from the development board. Any idea of what might cause the bad signal?