Other Parts Discussed in Thread: AM3352, TPS65910
Hi,
I'm designing a board using AM3352 where I will disable the RTC by pulling down RTC_XTALIN with a 10k resistor and connecting VSS_RTC to ground. Should RTC_PWRONRSTn be pulled down as well.
In order to not have to source CAP_VDD_RTC with an external 1.1V supply, I'll pull down RTC_KALDO_ENn and also provide 1.8V to VDDS_RTC.
The PMIC_POWER_EN output cannot be used because the RTC was disabled by not providing an input clock, even though the internal RTC_LDO will be on. Is this correct?
The power supply sequencing on page 95 of datasheet SPRS717D –OCTOBER 2011–REVISED MAY 2012 does not indicate any detailed information about how long the PWRONRSTn input should be asserted or if there is a minimum of cycles CLK_M_OSC must go before releasing the PWRONRSTn. I'm using a different power supply solution than the TPS65910.
Regards,
Elvis