This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About SD boot of DM8127.

Genius 3400 points


hi all, 

        Reference the IPNC 8127, we build our own board and start to debug. Using CCS, we can access the DDR3 correctly. But it cannot boot from the  SD-Card.

U-Boot 2010.06 (Oct 25 2012 - 14:32:54) DM8127_IPNC_3.00.00

TI8148-GP rev 2.1

ARM clk: 600MHz
DDR clk: 400MHz
L3 clk: 200MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP Default OFF
DSS Default OFF

DRAM: 512 MiB
MMC: OMAP SD/MMC: 0, ON-BOARD SDIO: 1
Using default environment

The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Hit any key to stop autoboot: 0
reading u-boot.bin

200532 bytes read
## Starting application at 0x80800000 ... 

It halt at the above line. 

Anybody can give me some advice?