Hi All,
We need to have CAN interface with AM335xEVM board and attached a PCAN cable (USB end connected to Ubuntu PC and CAN end connected to EVM). Since there is a CAN port provided with the EVM with ISO 1050 CAN controller, is there any readily CAN driver available with the Sitara Linux?
And if it is, whether CAN has implemented as character device or network device?
What are the necessary steps to receive data to CAN port of EVM ?
Any other suggestions would be appreciable. Thanking in anticipation.
Regards,
Mandar