Other Parts Discussed in Thread: OMAP-L138
Hello,
We are developping a custom board based on the OMAP-L138 SOC with a design closest as possible to the LogicPD da850evm board.
Main differences are :
- DDR2 instead of mDDR
- 83848 PHY chip instead of 8720 PHY chip without I2C stuff
- serial console available only on UART 0.
I am using the last psp : DaVinci-PSP-SDK-03.22.00.02.tgz.
I have modified succesfully U-Boot and it now works fine. It loads the Linux kernel uImage through TFTP and launch it.
The kernel hangs after :
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
I have done some modifications to Linux Kernel board-da850-evm.c file :
- add a davini_cfg_reg_list(da850_uart0_pins) call
- comment the __raw_writel(0, IO_ADDRESS(DA8XXX_UART0_BASE) + 0x30);
- in the da850_evm_console_init() function, set the preferred console at 0 instead of 2
In the U-Boot bootargs, I set the console to ttyS0.
I had configured the kernel to use the RMII PHY instead of MII.
I have enabled CONFIG_SERIAL_8250_CONSOLE in the kernel config Drivers section and
enabled CONFIG_DEBUG_LL in the Kernel hacking section.
I had also tried to replace, in the bootargs, the console=/dev/ttyS0 by console=uart,io,0xe1020000 without success.
Does the kernel reconfigure the memory controller ? (I have not find where).
Have I to apply the same modifications than that applied to U-Boot ?
Do I miss some modification needed to use the UART0 instead of UART2 allowing early kernel traces.Any help is welcome.
Thank you
Gilbert Brisset.