Other Parts Discussed in Thread: DM8107
Hi,
I am evaluating DM8107 for a decoder solution. Since there is no post category for DM810x and DM814x is similar to DM8107, I am posting in this forum
Any help on below will be highly appreciated.
1. Can the 8107 decoder auto reduce the frame rate once it overloaded with HW limitation (eg. I have opened 16 channels of 1080P@30fps with DM8107 and if decoder is not capable to handle this, will it still perform decoding of 16 channels, although at minimum frame rate ?(let's say 1 fps for each 16 channel ?))
2. If I have 16 channels of 1080P (although with 1 fps decoding of each) , can hardware scalar perform scale down operation of each channel to fit them in 4x4 layout ? What is the level of parallelism for 1080P input to scalar ? What is the maximum number of 1080P channels, h/w scalar can deal with at a particular instance ?
3. What is the limitation of input bit rate for decoder (considering case of 1x1080P_60, 4x720P_30 and 8xD1)? If the input channel's overall bit rate exceeds HW decoder's limitation, then what will happen ?
Regards,
Sweta