Which platform was the WEC7 example AM33X_OS included with the A8_2.30 BSP tested against?
It does not work with the official TI AM335X EVM kit.
Xloader runs but craps out when loading ebootsd.
Texas Instruments Windows CE SD X-Loader v0.0.0 for SubArctic 33X
Built Oct 28 2012 at 20:43:30
Version BSP_WINCE_ARM_A8 02.30.00.03
open ebootsd.nb0 file
Init HW: controller RST
SDCARD: requested speed 1000000, actual speed 1000000
SDCARD: requested speed 25000000, actual speed 19200000
read ebootsd.nb0 file
jumping to ebootsd image