The TSM320C6657 EVM has a compex PMBUS and VID controlled supply.
The PMBUS is connected to the FPGA which presumably programs it on power-up.
Is there any way to program it with default values using the fusion software and then store that in EPROM using the STORE_DEFAULT_ALL command,
alternatively are there any DC/DC converter modules with PMBUS and VID input that one could program up before fitting it to the board.
Would the default configuration of the UCD9222 cause excessive voltages or incorrect sequencing to occur ?
Could a jumper or DIP switch be used to disable the UCD9222 outputs prior to programming.
Finally, what would be the result of operating the VDDC at a fixed (non VID controlled) voltage ?