This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678: Unable to run different programs without a system reboot

Hello,

I am working with Advantech's DSPC-8681E PCIe card and their example CCS projects. After loading and running init.out for DDR3 initialization, I am able to run one of their examples correctly, but I am not able to run another example until I reboot the system. I have run into a similar problem with our own CCS project. After loading and running init.out, I can run our project once correctly, but I have to reboot the system to run it again. When I try to load and run the project again, it looks like the code does not even run on the DSP (no variables are set, HWIs and SWIs don't run, etc).

Has anyone else encountered this issue, and what possible solutions exist?

-Chris

Signalogic