Hi,
Describing a process:
1. I created the project of ccs4 for sharing with HAL one month ago.
When I want compile the code which was generated by HAL, I got a error :
>> Compilation failure
gmake: *** [source/system.obj] Error 1
gmake: Target `all' not remade because of errors.
2. I re-created the project of CCS4 for sharing with HAL again and update the HAL tools tool.
The code which was generated by HAL past the compiling and linking . So I thought I got mistakes when I created the sharing project.
After that time, Everything wes fine. If I changed some items, I can got the change in the code too.
3. I updated the HAL. There was a problem: when I change the setting item in HAL, the code did not change.
4. I created another sharing project. When I try to compile the code which come from HAL. I got same error information:
>> Compilation failure
gmake: *** [source/system.obj] Error 1
gmake: Target `all' not remade because of errors.
So I think the problem maybe come form HAL tools.
Is there some one can help me?
Thanks !
B.Rs,
Chuan