Other Parts Discussed in Thread: 4430
hi,
I type: make ARCH=arm uImage 2>&1 |tee ~/android_rls/mydroid/logs/kernel_make.out
and got the message below:
scripts/kconfig/conf -s arch/arm/Kconfig
can't copy type 0
CHK include/linux/version.h
UPD include/linux/version.h
CHK include/generated/utsrelease.h
UPD include/generated/utsrelease.h
Generating include/generated/mach-types.h
CC kernel/bounds.s
cc1: error: unrecognized command line option "-mlittle-endian"
cc1: error: unrecognized command line option "-mapcs"
cc1: error: unrecognized command line option "-mno-sched-prolog"
cc1: error: unrecognized command line option "-mabi=aapcs-linux"
cc1: error: unrecognized command line option "-mno-thumb-interwork"
kernel/bounds.c:1: error: bad value (armv5t) for -march= switch
kernel/bounds.c:1: error: bad value (armv5t) for -mtune= switch
make[1]: *** [kernel/bounds.s] Error 1
make: *** [prepare0] Error 2
How to solve it.
thanks!